hello every one
I Would like to know why ceramic and electrolyte capacitors are needed between vcc and gnd for a shift register 74hc595 while controlling dot matrix led segment
thanks
thulasi
hello every one
I Would like to know why ceramic and electrolyte capacitors are needed between vcc and gnd for a shift register 74hc595 while controlling dot matrix led segment
thanks
thulasi
What are water towers
They're needed to quickly supply current. Those chips will consume current in bursts and when that happens, if you don't have the caps to supply it, your VCC line will get pulled down a bit and that's going to generate a lot of noise on the rail.
Hello Razvan
Thanks for reply
why these capacitors are in parallel, what is their individual roll
Hey Thulasi, you should do a google on decoupling capacitors.
There's also a wikipedia entry which seems to do a pretty good job at explaining why they're needed: Decoupling capacitor - Wikipedia, the free encyclopedia
Razvan
Thanks for solution
With any digital circuit, noise is generated when the internal gates and other circuits switch from one state to an other, the faster the switching, usually means more noise. Power traces on a board are not perfect (0 Ohms) so therefore there is always a voltage drop along the trace, also there is inductance and capacitance to other nearby traces. decoupling capacitors are designed into the circuits to help manage this and provide easy paths of any noise generated to get back to ground rather than nearby signal traces
Noise is the "Interference" on the power and possibly other lines that if left un-checked can end up interfering with the normal operation of the circuit
larger electrolytic capacitors will provide low frequency decoupling and to a certain extent an additional source for short period increases of current requirements
the smaller ceramic caps (Or other material) are used for high frequency decoupling and will effectively provide a short to ground of this noise.
Why both, well Electrolytic are great for lower frequencies but internal construction tends to add inductance, series resistance and other factors that cause them to be less affective at the higher frequency ranges (capacitors are not perfect even though we would like them to be) so we add small value ceramic caps to provide the high frequency decoupling that the electrolysis can not handle