Arduino
  • Products
  • More
Arduino
Arduino Forum Shift register and Dot matrix led
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 419 subscribers
  • Views 848 views
  • Users 0 members are here
  • shift
  • register
Related

Shift register and Dot matrix led

e14 Contributor
e14 Contributor over 12 years ago

hello every one

 

I Would like to know why ceramic and electrolyte capacitors are needed between vcc and gnd for a shift register 74hc595 while controlling dot matrix led segment

 

thanks

thulasi

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    With any digital circuit, noise is generated when the internal gates and other circuits switch from one state to an other, the faster the switching, usually means more noise. Power traces on a board are not perfect (0 Ohms) so therefore there is always a voltage drop along the trace, also there is inductance and capacitance to other nearby traces. decoupling capacitors are designed into the circuits to help manage this and provide easy paths of any noise generated to get back to ground rather than nearby signal traces

     

    Noise is the "Interference" on the power and possibly other lines that if left un-checked can end up interfering with the normal operation of the circuit

     

    larger electrolytic capacitors will provide low frequency decoupling and to a certain extent an additional source for short period increases of current requirements

     

    the smaller ceramic caps (Or other material) are used for high frequency decoupling  and will effectively provide a short to ground of this noise.

     

    Why both, well Electrolytic are great for lower frequencies but internal construction tends to add inductance, series resistance and other factors that cause them to be less affective at the higher frequency ranges (capacitors are not perfect even though we would like them to be) so we add small value ceramic caps to provide the high frequency decoupling that the electrolysis can not handle

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    With any digital circuit, noise is generated when the internal gates and other circuits switch from one state to an other, the faster the switching, usually means more noise. Power traces on a board are not perfect (0 Ohms) so therefore there is always a voltage drop along the trace, also there is inductance and capacitance to other nearby traces. decoupling capacitors are designed into the circuits to help manage this and provide easy paths of any noise generated to get back to ground rather than nearby signal traces

     

    Noise is the "Interference" on the power and possibly other lines that if left un-checked can end up interfering with the normal operation of the circuit

     

    larger electrolytic capacitors will provide low frequency decoupling and to a certain extent an additional source for short period increases of current requirements

     

    the smaller ceramic caps (Or other material) are used for high frequency decoupling  and will effectively provide a short to ground of this noise.

     

    Why both, well Electrolytic are great for lower frequencies but internal construction tends to add inductance, series resistance and other factors that cause them to be less affective at the higher frequency ranges (capacitors are not perfect even though we would like them to be) so we add small value ceramic caps to provide the high frequency decoupling that the electrolysis can not handle