Arduino
  • Products
  • More
Arduino
Arduino Forum Operating HB100 backpack with Arduino Due
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 417 subscribers
  • Views 930 views
  • Users 0 members are here
  • speed-measuring
  • arduino
Related

Operating HB100 backpack with Arduino Due

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I need to connect a speed sensor module with an Arduino Due and calculate the speed of an approaching object.

 

the sensor is:

http://www.limpkin.fr/index.php?post/2013/08/09/Making-the-electronics-for-a-%247-USD-doppler-motion-sensor

 

The sensor already output a signal that its' frequency represents the speed of the object.

 

I would really appreciate any help understating how can it be connected and operated by the Arduino, and how can I sample its output?

 

If more details are needed I'll be happy to supply.

 

Thanks.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    Based on what you have provided I would say you have two choices

     

    1. Measure the frequency using an internal counter here is an examle: http://interface.khm.de/index.php/lab/experiments/arduino-frequency-counter-library/

    2. measure the voltage using the built in ADC here is an example http://arduino.cc/en/Tutorial/ReadAnalogVoltage or my own tutorial code here : http://www.element14.com/community/groups/arduino/blog/2014/06/10/fast-track-to-arduino-programming--lesson-3-improved-parsing-and-memory-usage-fully-working-programs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Thanks for the help.

     

    Can you please tell me where should I connect the module to the Arduino in order to operate it? Will connecting it to pin13 and set it to HIGH will do?

     

    I'm new to Arduino and am afraid I'll burn the sensor.

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    Do you have the device described in the video with the daughter card to condition the signals as shown in the video

     

    If so then pin 13 will not help you, you need to watch the video / articles I linked in above they also include how to connect the Arduino up. You also need to be sure the voltages are within the limits of the Arduino (5V) coming out of the sensor and you will need to supply power to the sensor as well so how much does it need

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    iI'm sorry but I can't see any video I these links.

     

    I have attached an image with the input and output of the sensor, it requires Vcc = 4.75V - 5.25V, Vout = 2.5 - Vcc.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    ok, that's good, do you know how much current it requires ?, if it is only a small amount then you could connect the 5V pin of the Arduino to it and of course the GND connection

     

    the output could go straight to one of the ADC pins (A0 - A5), these by default are configured to measure between 0-5V with a reading of 0 - 1023 after conversion. This is all clearly described in the link I gave above.

    http://arduino.cc/en/Tutorial/ReadAnalogVoltage or my own tutorial code here : http://www.element14.com/community/groups/arduino/blog/2014/06/10/fast-track-to-arduino-programming--lesson-3-improved-parsing-and-memory-usage-fully-working-programs

     

    follow those and you should be able to see something happening

     

    Regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    ok, that's good, do you know how much current it requires ?, if it is only a small amount then you could connect the 5V pin of the Arduino to it and of course the GND connection

     

    the output could go straight to one of the ADC pins (A0 - A5), these by default are configured to measure between 0-5V with a reading of 0 - 1023 after conversion. This is all clearly described in the link I gave above.

    http://arduino.cc/en/Tutorial/ReadAnalogVoltage or my own tutorial code here : http://www.element14.com/community/groups/arduino/blog/2014/06/10/fast-track-to-arduino-programming--lesson-3-improved-parsing-and-memory-usage-fully-working-programs

     

    follow those and you should be able to see something happening

     

    Regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    It requires 50mA so I guess it's ok.

     

    Thanks a lot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    yup, that should be ok