Arduino
  • Products
  • More
Arduino
Arduino Forum The Arduino Automated Sentry Turret (AAST)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 573 views
  • Users 0 members are here
  • helpme
  • electrical
  • arduino
Related

The Arduino Automated Sentry Turret (AAST)

e14 Contributor
e14 Contributor over 12 years ago

I'm working on a turret that doesn't require a laptop for operation. This of course means that the turret won't be as advanced when it comes to targeting.

 

This turret will run on the Arduino Uno R3.

The reason why I'm not using a more advanced board is because I'm trying to focus on a more simplistic, inexpensive schematic.

 

Here's the list of things I'm using for this:

-------------------------------------------------------------------------------------------------------

1x Arduino board

1x Ping Distance Detector (Used for left-to-right or right-to-left targeting)

1x PCB

1x Electric Airsoft Mechanism

1x Power N-Channel MOSFET

image1x Servo

??? (A section to fill in for stuff I probably forgot to put in this list)

-------------------------------------------------------------------------------------------------------

 

Well, I haven't thought everything through. This is mostly being improvised, so I imagine that there's probably a TON to fix and add.

 

I'm just throwing this idea out there. Yes, I know that it's been done before, but I'd like some input. I'm a rookie, after all.

NOTE: Reminders or suggestions are labeled with: image

  • Sign in to reply
  • Cancel
Parents
  • kidiccurus
    kidiccurus over 12 years ago

    You probably need a servo to move the turret left and right. Also, if you can persuade the other team to wear an infra red source then a wiimote sensor can give you x and y coordinates. See this instruct able for details m.instructables.com/id/Wii-Remote-IR-Camera-Hack/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kidiccurus
    kidiccurus over 12 years ago

    You probably need a servo to move the turret left and right. Also, if you can persuade the other team to wear an infra red source then a wiimote sensor can give you x and y coordinates. See this instruct able for details m.instructables.com/id/Wii-Remote-IR-Camera-Hack/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to kidiccurus

    Oh god, that's right!

     

     

    I have a servo specifically for this, and I completely forgot to add it to this list!

     

    Thanks for the reminder!

     

    As for the Wii mote sensor idea, I'll look into it.

     

    Thanks,

     

     

    Johnny.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kidiccurus
    kidiccurus over 12 years ago in reply to e14 Contributor

    Glad I could help.