Arduino
  • Products
  • More
Arduino
Arduino Forum How to go about re purposing  an 80's boom-box
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 417 subscribers
  • Views 788 views
  • Users 0 members are here
  • bluetooth
  • purpose
  • in
  • audio
  • boombox
  • boom
  • box
  • noob
  • :3
  • re
  • arduino
Related

How to go about re purposing  an 80's boom-box

e14 Contributor
e14 Contributor over 12 years ago

Easiest way i could think about doing it would to use the lleft and right wiring of the rradio so the audio out of the radio would be replaced by an aux in jack, or ahould i take everything out except the speakers, put in my own power system and amp,arduino as my controller, and even bluetooth shield,  still kinda noobish but if anyone wants to help me i could post some pictures  of the boom box disassembled, but im fairly certain ive located the radio part and and maybe the radio audio out,

 

 

(also want to put one of those led matrix sound level bar things in the radios window, to give it a cool vibe since i pooped up the tuning system :3 )

*and the dual cassete deck was broken so lots of empty sapce and room to play around

  • Sign in to reply
  • Cancel
Parents
  • rwslaugh
    rwslaugh over 12 years ago

    Just curious, but what are you putting inside to generate the new audio?  Sounds like a good possibility to drive it with a Pi, then add wireless if needed and put the whole MP3 library on board....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rwslaugh

    i thought amps drove the sound, and i would just take the sound from my smart phone or mp3 player by wither having an aux jack in and later add in a bluetooth shield (either from retail or program my own shield, most likely with an atmega 328, )

     

    *btw the speaker DID have an "in" but only playble through the 2nd casstte deck, whcih muffled the sound and dident utilize the speakers fully, then switching to radio the sound quality, bass, and eveything sounds amazing, so thats why im having todo this hack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rwslaugh
    rwslaugh over 12 years ago in reply to e14 Contributor

    Yes, sorry, amps would drive the sound.  My approach was using a Pi or some uP board to add a level of control and network capability.

    If all you are doing is driving the speakers then a small amp is all you need - with a line input you can connect to your other items.  The bluetooth connectivity does come with some amps so you should be able to find some.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rwslaugh

    okay cool, another q, is would i use my own power system or use the power system that comes with the boom box? and if the amp has its on power would it be enough for my speakers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rwslaugh
    rwslaugh over 12 years ago in reply to e14 Contributor

    For the power system question..it depends on all the voltages needed and if it has the outputs for such.  As for the power to push the speakers, how many watts does the amp supply and to what type of load?  Typically the load is a certain number of 8 ohm speakers.  The boom box probably has two large 8 ohm and maybe a few more smaller ones. ("woofers", "Tweeters")  Do you know how many watts the amp can supply?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rwslaugh

    hey thi sproject isent dead i havent had time to work on it, but ill reply once i can get back to it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to rwslaugh

    hey thi sproject isent dead i havent had time to work on it, but ill reply once i can get back to it