Arduino
  • Products
  • More
Arduino
Arduino Forum Home automation project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 418 subscribers
  • Views 1065 views
  • Users 0 members are here
  • Design
  • arduino
Related

Home automation project

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

This is my first post here at element 14. I hope this is one of the best places i can seek help regarding all things electronics. I basically have an idea but not quite sure how to start about it. I have researched the internet and alot of people are loving the Arduinos. I myself enjoyed the tutorials made by Jeremy Blum so am leaning towards using them for this project.

 

So i want to make a simple home automation project. With the following features:

 

Each room will have a controller board powered by a microcontroller. This room controller will have a keypad, an LCD, an IR and a Temperature sensor interfaced. When i click buttons from the keypad, it basically turns on/off the lights. I want to try first with 8 lights (hence 8 buttons). Furthermore i would like two dimmable outputs meaning light or fan that i can dim (increase/decrease power). For this i wanted two sets of two buttons (4 in total). One set to increase and one to decrease the power for one output and the second set for the second one.

Same keypad will be mapped on an IR remote so that these switches can also be controlled from there.

 

I want 3 ~ 4 controllers like the one described above (can be exact clones) so i can put in other rooms.

 

All these controllers will be networked together and a master controller will receive their switch status and  change it via a computer as well.

 

 

In the past i have made something similar but on PIC microcontrollers and was like 5 years ago. I want to move to the latest technology image

 

Can anyone shine some light on this project or if have worked on something similar let me know some of the issues they faced.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Hassan,

     

    there are also some arduino-home-automation-projects that use xbee-shields for communication. This could be an alternative to the Pi. And there are also keypad-shields for the arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Hassan,

     

    there are also some arduino-home-automation-projects that use xbee-shields for communication. This could be an alternative to the Pi. And there are also keypad-shields for the arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks Marc, can you please share a link to that post/project ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    http://www.instructables.com/id/myHome-temperatureoilelectricity-monitoring-wi/?lang=de

    http://www.makechronicles.com/2012/06/08/arduino-project-10-2d3d-pictures-my-xbeearduino-based-wireless-sensor-network-unomega-2560-1-0-xbee-series-2/

     

    They are a bit different from what you are talking about but go in the same direction. Basically it's always the same:

     

    - gathering inputs from temperature sensors, humidity sensors, motion detectors, buttons,...

    - control outputs: servos, leds, lcds, lights,...

    - arduino as the main plattform

    - xbee for wireless communication

    - no special timing requirements (you don't care if your lights turn on after 1 or 10 ms...)

     

    Here are some information about your wireless options:

    http://www.openhomeautomation.net/wireless-home-automation/

     

    I looked into this topic a bit for myself, but as I'm quite new to this topic, I maybe should start with something smaller and easier. image

     

    Good lock with your project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks Marc. I am looking into the links you sent me.