Arduino Forum Mux Shield error on example
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
  • Replies 7 replies
  • Subscribers 393 subscribers
  • Views 572 views
  • Users 0 members are here
  • mux
  • shield
  • muxshield
  • arduino
Related

Mux Shield error on example

Former Member
Former Member over 10 years ago

Hello everyone,

I've bought a Mux Shield II and I'm trying to test it on an Arduino Mega 2560.

 

I've downloaded the libary and put in libraries folder just exactly how it's explained into User Guide,

 

The error is in the initializing  of the shield:

 

image

How you can see from the image, the shield is not even recognized as type of variable.

In userGuide I can find:

image

I've also tried to implement:

MuxShield() muxShield;

using the parentesys but I got the same error.

 

Can someone help me?

Thank you very much!!!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to bobcroft +1
    My experience with having a library in twice is it starts to give errors but not stating the real problem, I cannot remember the exact error and im not in a position to try right now Suffice to say… don…
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes +1
    Thank you all guys, I removed the double library folder and just put it into Programs> Aduino>libraries Then I REMOVED THE FOLDER "_MACOSX".... So from: Programs> Aduino>libraries>MuxShield>_MACOSX MuxShield…
Parents
  • gadget.iom
    gadget.iom over 10 years ago

    Hello Alessandro.

     

    Have you installed the library?

    It needs to reside in the Arduino/Libraries directory before it can be used.

    Just copy the entire MuxShield directory over and then restart the Arduino IDE.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to gadget.iom

    Hi Paul,

    yes, I've done it

    image

     

    And I've restarted te IDE various times, but it doesn't work. I don't really figure out the reason :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to gadget.iom

    Hi Paul,

    yes, I've done it

    image

     

    And I've restarted te IDE various times, but it doesn't work. I don't really figure out the reason :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gadget.iom
    gadget.iom over 10 years ago in reply to Former Member

    Do you have an Arduino directory in "My Documents"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to gadget.iom

    Yes, I have, and after th error, I've put the library there also.

    image

    image

     

    The double directory is due to the presence of the library in both Programs>Arduino>librariers and also into Documents>Arduino>libraries.

     

    But this ad I've done only after the error (restarting the IDE) many and many times...