Arduino Forum Has anyone ever controlled a HD video camera using an Arduino?
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
  • Replies 4 replies
  • Subscribers 402 subscribers
  • Views 413 views
  • Users 0 members are here
  • videobooth
  • control
  • ap:digital_video_recorder
  • arduino
Related

Has anyone ever controlled a HD video camera using an Arduino?

Former Member
Former Member over 10 years ago

Hi everyone,

 

I'm getting married this summer and I would really like to build a DIY Video Booth, where I would enclose a video camera and controller. The idea would be that people would come into the video booth, press a START button which would light up the booth and start a 3 second countdown after which the video would begin recording. The recording would last 20 seconds or so. I would also like a screen or iPad to connect to the recorder which would face the person so they could see themselves in the frame and also display instructions of use, countdown, thank you message etc. I've no doubt this can be done but can anyone steer me in the right direction with it?

 

Thanks so much in advance

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 10 years ago +1
    Hi! Does it need to be Arduino? Personally, I would probably tackle such a project using a Raspberry Pi. There is an HD camera module available for it, buttons could be connected to the GPIO pins and an…
  • fvan
    fvan over 10 years ago

    Hi! Does it need to be Arduino?

     

    Personally, I would probably tackle such a project using a Raspberry Pi. There is an HD camera module available for it, buttons could be connected to the GPIO pins and an HDMi screen could be connected for the preview. The pictures would be stored on the Pi's SD, which you could potentially make available via wifi/bluetooth.

     

    Just a thought image

     

    Frederick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to fvan

    Hi Fredrick

     

    That sounds like exactly what I need. Are they difficult to program? Do you know of any good sites that could help me with it?

     

    Many thanks

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to fvan

    Hi Fredrick

     

    That sounds like exactly what I need. Are they difficult to program? Do you know of any good sites that could help me with it?

     

    Many thanks

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fvan
    fvan over 10 years ago in reply to Former Member

    Hi John,

     

    searching for "Raspberry Pi Photo Booth", I've come across several tutorials/guides. This one seemed very interesting: http://www.drumminhands.com/2014/06/15/raspberry-pi-photo-booth/

     

    Frederick