Arduino Forum How to program USB host shield?
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
  • Replies 10 replies
  • Subscribers 403 subscribers
  • Views 2140 views
  • Users 0 members are here
Related

How to program USB host shield?

Former Member
Former Member over 10 years ago

Hello

I need your help as soon as possible.

I have a Arduino Mega board and a USB host shield (like this : http://www.ebay.es/itm/like/261880660401?limghlpsr=true&hlpht=true&ul_noapp=true&hlpv=2&chn=ps&lpid=115&ops=true&viphx=1).

I need send some information from PC using Serial communication to Arduino mega by its programing port, and send this information by the USB host shield using Serial communication too.

It must run like a bridge, I send information from pc this information passes through the board and it is sent through the USB host shield.

 

 

PC=======>Arduino MEGA====>USB HOST SHIELD=====>OTHER MACHINE

 

 

All using serial communication.

 

 

It seems easy, but I couldn't find someone who tell me how I could do it.

I need some example code or something. It is very important because I need do it for a work.

Sorry for my English.Thanks in advanced

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago in reply to Former Member +1
    Understood - The post that Clem left has excellent information on using the USB Host Shield; especially some gotchas with clocking the data. Here is the Github link for the shield (lots of example code…
Parents
  • Former Member
    Former Member over 10 years ago

    I have an arduino mega 2560 board, i need send information from a windows pc to arduino mega 2560 by the programming port using serial communication, this part is solved, but when an specific kind of information is sent, this information must be sent to other device using the USB host shield and serial communication too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Understood - The post that Clem left has excellent information on using the USB Host Shield; especially some gotchas with clocking the data.  Here is the Github link for the shield (lots of example code): https://github.com/felis/USB_Host_Shield_2.0

    and a specific link to outputting data from that shield (that includes code): http://mitchtech.net/android-arduino-usb-host-simple-digital-output/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Understood - The post that Clem left has excellent information on using the USB Host Shield; especially some gotchas with clocking the data.  Here is the Github link for the shield (lots of example code): https://github.com/felis/USB_Host_Shield_2.0

    and a specific link to outputting data from that shield (that includes code): http://mitchtech.net/android-arduino-usb-host-simple-digital-output/