Arduino Forum Could I just push these pins into a breadboard?
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
  • Replies 4 replies
  • Subscribers 403 subscribers
  • Views 550 views
  • Users 0 members are here
  • wifi
  • pins
  • transceiver
  • breadboard
  • arduino
Related

Could I just push these pins into a breadboard?

Former Member
Former Member over 10 years ago

ESP8266 ESP-01 Remote Serial Port WIFI Transceiver Wireless Module Sale-Banggood.com

 

I was looking at this lovely wifi serial transceiver module when I looked at the picture of the pins. There are 8 pins but they are in rows of 4. The seems pretty strange and I couldn't just put it into a breadboard could I? If I couldn't would I have to solder wires onto the pins and hook it up that way? I would really prefer not to go there. Anyways I would love the help. Thank you in advance. image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    cant just plug into the bread board as there is no where to separate the two rows, there too close together what I do is use a female to female jumper leads and push header pins into the breadboard to…
Parents
  • Former Member
    Former Member over 10 years ago

    Thanks guys! Those links helped a lot. And that female jumper idea is genius!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago

    Thanks guys! Those links helped a lot. And that female jumper idea is genius!