Arduino
  • Products
  • More
Arduino
Arduino Forum MQTT client program not showing any results with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 420 subscribers
  • Views 6419 views
  • Users 0 members are here
Related

MQTT client program not showing any results with Arduino

e14 Contributor
e14 Contributor over 11 years ago

I modified the MQTT example present under MQTT library pubsubclient for Arduino.

My MQTT server address is 192.168.1.6 with port 8081.

To this MQTT server,another MQTT client in my mobile is able to connect.

But this is not working with Arduino.There is no error shown during compilation or during uploading.

Infact,I am not able to see the connection result messages such as "Connected" or "Not connected" which i given in Serial.println() in setup function.

I am resetting Arduino before uploading the program.Please let me know why this is not showing any output....

 

#include <SPI.h>

#include <Ethernet.h>

#include <PubSubClient.h>

// Update these with values suitable for your network.

byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

byte server[] = {192, 168, 1, 6 };

//byte ip[]     = { 172, 16, 0, 100 };

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

EthernetClient ethClient;

PubSubClient client(server, 8081, callback, ethClient);

void setup()

{

  Ethernet.begin(mac);

  if (client.connect("*")) {

     Serial.begin(9600);

    Serial.println("Connected to MQTT Server");

    client.publish("outTopic","hello world");

   // client.subscribe("inTopic");

  }

  else

  {

   Serial.println("Could not connect to MQTT Server");

  }

}

void loop()

{

  //client.loop();

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 11 years ago in reply to e14 Contributor +3
    generk4 and organtin Hi Radhamani and Giovanni - I had 30 minutes to spare so I copied the program from comment 19 and posted it into the Arduino IDE (I am using 1.6.1), compiled and uploaded it to a genuine…
  • e14 Contributor
    e14 Contributor over 11 years ago +3
    Hi Bob, Neil and Clem, I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me I am sooo happy Thanks once again for your wonderful support and help
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobcroft +2
    Hi bob,Neil,Clem and many others who have helped and guided me in this issue, I have successfully completed MQTT program and Arduino is successfully publishing and subscribing messages Next step,I am going…
Parents
  • organtin
    organtin over 11 years ago

    As the author of the suggested post, I add here few hints (besides those I sent privately by email).

     

    Install the sketch suggested by Clem Martins to your Arduino: just change the PORT from 5000 to 23. Then use any telnet client to try to connect to the Arduino. If it answer you are done.

     

    The telnet client, as well as the correct set of parameters to be used, depend on your network and OS configuration. If you own a Linux or a MAC OS X box, just open a terminal and type

     

    telnet xxx.yyy.zzz.hhh

     

    where xxx.yyy.zzz.hhh is the IP address of the Arduino. If you have a Windoze box find some tutorial searching for "telnet for windows 8" in google (for windows 8).

     

    You can get the appropriate parameters to configure your network using /sbin/ifconfig in a terminal in Linux of MAC OS X. For mine, e.g., this reads

     

     

    eth0      Link encap:Ethernet  HWaddr aa:bb:cc:dd:ee:ff

              inet addr:ggg.hhh.iii.jjj  Bcast:kkk.lll.mmm.nnn  Mask:ooo.ppp.qqq.rrr.sss

              inet6 addr: [...omissis...] Scope:Link

              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

              RX packets:21735485 errors:0 dropped:0 overruns:0 frame:0

              TX packets:11473256 errors:0 dropped:0 overruns:0 carrier:0

              collisions:0 txqueuelen:1000

              RX bytes:5803016757 (5.4 GiB)  TX bytes:10549063051 (9.8 GiB)


    Here, what you need, is kkk.lll.mmm.nnn to be used as the gateway and ooo.ppp.qqq.rrr.sss as the mask. To get your DNS, just type


    dig google.com


    At the end you will see


     

    ;; Query time: 33 msec

    ;; SERVER: 141.108.35.4#53(141.108.35.4)

    ;; WHEN: Mon Mar 16 16:18:35 2015

    ;; MSG SIZE  rcvd: 116


    141.108.35.4 is the DNS.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to organtin

    Thanks much for your guidance..

     

    This is the output of dig google.com

    ;; Query time: 31 msec

    ;; SERVER: 203.145.184.32#53(203.145.184.32)

    ;; WHEN: Mon Mar 16 23:25:56 2015

    ;; MSG SIZE  rcvd: 204

     

    ==================================

    Here is the excerpt from the output of ipconfig/all

     

      Default Gateway . . . . . . . . . : 192.168.1.1

      DHCP Server . . . . . . . . . . . : 192.168.1.1

      DHCPv6 IAID . . . . . . . . . . . : 319607442

      DHCPv6 Client DUID. . . . . . . . : 00-01-00-01-1A-0F-5B-36-20-1A-06-34-92-D3

      DNS Servers . . . . . . . . . . . : 203.145.184.32

    =======================================

    I used the below code from the link you have mentioned,

     

    #include <Ethernet.h>

    #include <SPI.h>

    #define PORT 23

    byte mac[] = {0x5e, 0xa4, 0x18, 0xf0, 0x8a, 0xf6};

    IPAddress arduinoIP(192, 168, 1, 67);

    IPAddress dnsIP(203, 145, 184, 32);

    IPAddress gatewayIP(192, 168, 1, 1);

    IPAddress subnetIP(255, 255, 255, 0);

     

    EthernetServer server(PORT);

    boolean notYetConnected;

     

    void setup() {

      Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);

      notYetConnected = true;

    }

     

    void loop(){

    }

    ======================

    Results of telnet:

    C:\Users\Radhamani>telnet 192.168.1.67 23

    Connecting To 192.168.1.67...Could not open connection to the host, on port 23:

    Connect failed

     

    image Still not working..I am so worried.Not sure where it is going wrong..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    I am from India..Actually I am doing my college project and in only 2 more weeks I have to submit the project.And due to Ethernet shield issue,I am stuck with the project.Earlier I ordered in Ebay ,but they said they have ran out of stock.

    I am thatswhy trying to get the Shield directly from Electronics labs due to less time.

     

    I am planning to buy "PoEthernet Shield, cmostronics".Could you please suggest whether this component is right one for Arduino UNO?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    generk4 Hi Radhamani.  As far as I can see it looks OK. The tutorial does use an Arduino UNO.

     

    Are you complicating things by going for POE, or is that part of your project?

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    Hi Neil Kenyon,Actually my project is to use a sensor to act as one of MQTT clients to communicate with IBM MessageSight which acts as MQTT Server to publish and subscribe messages.

    To achieve this scenario,I am using Ethernet shield to first gain an IP and then use similar setup as that of " A Simple Example (Arduino, MQTT, m2m.io) - m2mio " to achieve MQTT scenario.

    I am stuck up in the initial stage itself in setting up IP for Arduino due to issue in Ethernet shield configurations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    generk4  Hi Radhamani sorry I can't offer any more suggestions, other than a faulty Ethernet Shield.

     

    Hope you can get it sorted out

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to neilk

    No problem Neil.Today I will be getting new Ethernet shield which will be working one.Then I will try the code and update.

    Thanks much for your help so far image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 11 years ago in reply to e14 Contributor

    Radhamani,  glad to hear you are getting a  new shield.  I have been away for a few days and unable to post.  When you get your new shield please try the example sketch i Arduino 1.6.1, Ethernet folder, sketch is called DhcpAddressPrinter.  Plug your shield onto your Arduino UNO and power via the USB cable.  Upload the sketch and run it.  Open the Arduino terminal window and make sure it is set to 9600 baud.  Unless you have a genuine Arduino Ethernet shield then it will NOT have a sticker giving the shields MAC address so the default MAC address in the sketch should work.  You can also choose your own MAC address as long as it follows the same format as the example.

     

    If you get a print out of the automatically assigned IP address for the shield, SUCCESS! you can then progress to getting your MQTT code working.  Please do try the example sketches because these are known to work.  Once you have the DHCP sketch working you can try pinging that IP address and you can then try setting the IP address manually, again follow some of the example code given.  Remember that IP addresses of the form 192.168.1.xx or similar are on your local net work and not accessible to the WAN without port forwarding unless you have a static IP.

     

    If you cannot get an IP address for the shield either manually or automatically and everything is powered up correctly and the Ethernet cable is good then you could have a problem with your router or the UNO.  Do you have a friend where you could take your set up and try it on their system or at university / college?

     

    I'll keep my fingers crossed that your new shield works and you are able to make progress.

     

    Bob

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobcroft

    Thank you so much bob for your support on this..I am feeling very happy and confident when I am getting so much help and guidance from you all in this forum.:)

    I am trying the example now with new UNO and Ethernet shield.Will let you know the progress

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hurrah!!! It seems to be working...

    imageimage

    After replacing the components,

    Starting ethernet...192.168.1.67 is showing in Serial monitor

    And,

    C:\Users\Radhamani>ping 192.168.1.67

     

     

    Pinging 192.168.1.67 with 32 bytes of data:

    Reply from 192.168.1.67: bytes=32 time<1ms TTL=128

    Reply from 192.168.1.67: bytes=32 time=1ms TTL=128

    Reply from 192.168.1.67: bytes=32 time=45ms TTL=128

     

     

    Ping statistics for 192.168.1.67:

        Packets: Sent = 3, Received = 3, Lost = 0 (0% loss),

    Approximate round trip times in milli-seconds:

        Minimum = 0ms, Maximum = 45ms, Average = 15ms

     

    Hope next I can start with MQTT program.. image

     

    (Anyhow,telnet 192.168.1.67 80 showing connection failed!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to e14 Contributor

    generk4  Hooray!!!!!!!!!!!!!!!!!!!!!!!!!!! image

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 11 years ago in reply to e14 Contributor

    Fantastic news!!!  I suggest you save a copy of each stage that works as you develop your code.  That we you only have to go back one step when you hit a snag.  I couldn't get TELNET working either!  You shouldn't have any problems with MQTT  now you have a working Ethernet card and IP address.

     

    Bob

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobcroft
    bobcroft over 11 years ago in reply to e14 Contributor

    Fantastic news!!!  I suggest you save a copy of each stage that works as you develop your code.  That we you only have to go back one step when you hit a snag.  I couldn't get TELNET working either!  You shouldn't have any problems with MQTT  now you have a working Ethernet card and IP address.

     

    Bob

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobcroft

    Hi bob,Neil,Clem and many others who have helped and guided me in this issue,

    I have successfully completed MQTT program and Arduino  is successfully publishing and subscribing messages image

    Next step,I am going to use Dallas Temperature sensor (DS18B20) as one of MQTT clients... image Lets see how it goes image

     

    Thanks a lot for all your support image .Without your guidance,this would not have been possible for me ...