Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino + object avoidance robot.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 417 subscribers
  • Views 2135 views
  • Users 0 members are here
  • robotics
  • arduino
Related

Arduino + object avoidance robot.

dtsartsanis
dtsartsanis over 11 years ago

Hi everybody.

 

Few days now i started building a small robot (my first one) using an arduino as a controller.

This post is a small presentation of this project

 

The kit of the robot is from Actobitty and it is a simple 2 motor with an aluminum chassis.

The front "wheel" was a simple plastic one and i noticed that it was difficult to overcame small objects and also difficult in turning. So i took pieces from an old Lego Technic and i made a front fork.

 

this was the front wheel and these are the holders of the battery below the chassis. I also removed them and manage to transfer the battery up.

image

 

this is the Lego fork

image

 

 

this is how the robot looked when i assembled it.

image

 

and this is how it looks now.

image

 

The original kit includes two holders for your Arduino or Raspberry. I manage to put the breadboard with the holders.

Also the battery pack moved in front of the micro controllers.Now there is a small space at the end of the breadboard for connecting leds etc.

 

Now the robot uses the following parts:

1.Actobitty 2 wheels robot aluminum chassis

2.2x Micro Gearmotor - 90 RPM

3.Arduino Uno

4.Arduino Motor shield rev.3

5.Ultrasonic sensor HC-SR04 with bracket

6.Breadboard for prototyping and additional sensors.

7.Additional 9V battery.

8.Cell AA Battery Pack with 4 rechargeable batteries

 

This is a the how u can attach the second battery.

image

 

At the present the robot can avoid objects and i found a very good tutorial here James Robot Tutorial - Duino-Robotics .

The code from the tutorial is for a robot with a servo ultrasonic sensor and servo motors. I use an Arduino motor shield so i had to make modifications.

 

In the next days ill try to load a video with the robot in action.

 

*the attachment code is working for me but still needs improvement

Attachments:
sample_code_for_robot.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 11 years ago +3
    dtsartsanis Hi Dimitrios - a very nice piece of work! Well done. The code looks very useful for my own Cybot project. Are you going to include a way of sending commands to your robot? I am working on using…
  • mcb1
    mcb1 over 11 years ago +3
    Dimitrios Nice project. The ping sensor may not be seeing the echo from the door, and as I understand not all ping sensors are equal. To overcome the front wheel issues, I've tended to build tail draggers…
  • dtsartsanis
    dtsartsanis over 11 years ago +2
    A small modification to the 9V battery. It stays at the back of the chassis with tie zips. The good about the Actobity chassis is that it has a lot of holes and you can attach either sensors or whatever…
Parents
  • dtsartsanis
    dtsartsanis over 11 years ago

    Today i tested various different times of scaning with the ultrasonic sensor.

    The main set up is :

    1. maxdistance 100 (10cm) this is the scanning distance

    2.delay of the scan with the sensor 300 in milliseconds

    3.frontdistance >20 which means if the scan gives 20 and above go forward

     

    Also managed to find how to turn right and left with the code if the distance of the object is below 5 turn right or below 5 turn left.

    I dont know why but when the sensor points the door which is wooden and shiny the robot have some problems. if the robot is in an angle with the door usually it hits the door.

     

    If i could lower the sensor the movement would be better but for now i am very happy with the whole progress.

    The blue led is blinking when the robot go backward and a good idea is to add a piezo buzzer to make a sound also when it goes backward like the trucks.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Attachments:
    2678.sample_code_for_robot.ino.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dtsartsanis
    dtsartsanis over 11 years ago

    Today i tested various different times of scaning with the ultrasonic sensor.

    The main set up is :

    1. maxdistance 100 (10cm) this is the scanning distance

    2.delay of the scan with the sensor 300 in milliseconds

    3.frontdistance >20 which means if the scan gives 20 and above go forward

     

    Also managed to find how to turn right and left with the code if the distance of the object is below 5 turn right or below 5 turn left.

    I dont know why but when the sensor points the door which is wooden and shiny the robot have some problems. if the robot is in an angle with the door usually it hits the door.

     

    If i could lower the sensor the movement would be better but for now i am very happy with the whole progress.

    The blue led is blinking when the robot go backward and a good idea is to add a piezo buzzer to make a sound also when it goes backward like the trucks.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Attachments:
    2678.sample_code_for_robot.ino.zip