Arduino Forum Servo Problem
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
  • Replies 7 replies
  • Subscribers 403 subscribers
  • Views 472 views
  • Users 0 members are here
  • pwm
  • servo
Related

Servo Problem

rishi2628
rishi2628 over 10 years ago

i have a custom avr atmega328 board to which two seven segment, a servo and a crystal with capacitor is attached. when only the seven segment is connected, the microcontroller works perfectly.But when i attach the servo along with the seven segment, it starts blinking very rapidly and the servo moves to the extreme end. i have programmed the servo to rotate 0 to 90 and then 90 to zero and the seven segment to show its angle. My code is fine, i have verified it using the arduino. i guess the crystal is causing some interference or there is anything else needed for the pwm operation that i am missing to use the servo. can anyone help me out...??????.....please!!!

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +4
    Where is the power for the servo coming from? A diagram of connections would help greatly. a meter showing current would help if you have one handy. Clem
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +4
    Can you provide schematic to show how everything is connected and also the sketch, this will allow us to hep you better
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Can you provide schematic to show how everything is connected and also the sketch, this will allow us to hep you better

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Can you provide schematic to show how everything is connected and also the sketch, this will allow us to hep you better

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rishi2628
    rishi2628 over 10 years ago in reply to Robert Peter Oakes

    here is the schematic.................i tried simulating it......................the pwm pin (15th pin) is continuously on in the simulation ............. but when i make the same circuit using an arduino.............it works perfectly.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to rishi2628

    Well a lack of capacitors on the crystal immediately raise concerns. The reliable timing of your PWM will most likely rely on capacitors being in place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rishi2628
    rishi2628 over 10 years ago in reply to gadget.iom

    i have attached the capacitors...22pf.....i just forgot to show them in the schematics