Arduino Forum How to offer job for board and LED design?
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
  • Replies 9 replies
  • Subscribers 390 subscribers
  • Views 443 views
  • Users 0 members are here
Related

How to offer job for board and LED design?

Former Member
Former Member over 10 years ago

I am very sorry if this is not the correct place for this question.

 

I am a machinist and manufacturer of a motorcycle throttle lock and recently purchased some boards for displays that read a pot from an electric bicycle throttle and use that information to light up a series of LEDs that are mounted on the board. Basically it is an RPM gauge.

 

Unfortunately the LEDs are very dim and I am hoping to have a few boards made that I can use to light much brighter LEDs. I know 3D design, CAM, G-Code and machining, but electronics are a foreign language to me. There are a few other design considerations and constraints but I was poking around and saw the Arduino Nano and love the small form factor since ideally this needs to fit into a small mirror housing.

 

Free time isn't something I have in large supply and would prefer to pay for help to design vs. buying a bunch of stuff and playing/testing/learning as I don't have any other known usages for digital boards and learning to program them.

 

I appreciate anyone's time for reading. Perhaps pointing me to information or someone interested in doing the design.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Hi Brian, One thing you might try is simply replacing the LEDs on the cards you have with brighter devices. Any LED with a brightness rating over 1000 millicandellas will be visible in direct sunlight…
  • shabaz
    shabaz over 10 years ago +1
    I agree with Andy, it should be straightforward to swap the LEDs out. Those arrays are a bit tricky to desolder but there are tools for that. There is also a single resistor (two in your case since the…
  • Former Member
    Former Member over 10 years ago +1
    Thank you guys. These are not going to go on-bike but merely sit on a counter at a motorcycle dealership so customers can't watch the display and play along to learn how to use the product. I was under…
Parents
  • dougw
    dougw over 10 years ago

    Hi Brian,

    One thing you might try is simply replacing the LEDs on the cards you have with brighter devices. Any LED with a brightness rating over 1000 millicandellas will be visible in direct sunlight - obviously most automotive LEDs work in sunlight. It will not hurt the circuit to have brighter LEDs installed, assuming they are the same color. You may need to install a switch to reduce brightness at night or add a slightly more complex circuit to automatically dim in low ambient light.

    If you want to have a module built, you probably don't need a microcontroller like an arduino.

    For example a single chip like an LM3914 can convert an analog voltage or pot output into a 10 LED bargraph. The schematic in the datasheet may be adequate for your application.

    A little ,more info would be useful in optimizing he design

    - how big should the PCB be?

    - how may LEDs?

    - what color?

    - what signal controls the number of LEDs?

    etc.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to dougw

    These boards cost me $70 each which is WAY to expensive for what I need. Replacing these LEDs would seem to be a poor investment.

     

    Pictures attached. The board is 2.5" x 1.75" the 1.75" is perfect for this case and would be most convenient to stay equal or less than that.

     

    There are 20 LEDs on this board 4 of which always stay on. 10 LEDs would be plenty if only the first one stayed on. Red LEDs are perfect but I'm not really hung up on the color.

     

    These are point of purchase displays for dealerships. I am going to have a digital picture frame behind the display so I ideally the board would be able to share the power supply from the picture frame. the one in the picture uses a 5V___1000ma supply so 5V would be ideal, however I can try to find something else.

     

    I'm not stuck on the Arduino, but definitely need something better than what I have now.

     

    Just kidding on the pictures. I am going to have to retake them or scale them way down to upload here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to Former Member

    Hi Brian, it looks like you've got the bar graph chip Doug mentioned. If it is to go on a bike then I'd swap out those sockets and solder the chips directly but if it's to be office based then that's not an issue.

     

    To be honest $70 for a a small batch of boards is not a bad price. You will find that the costs are not due to the selection / number of components but the design and assembly time. If you have thousands to make then you should be able to get the unit cost down. I'd have thought you could swap the LED array out with high brightness LEDs, either thru hole or surface mounted to solve the light problem and reduce the part costs. If you can't change the board then you could have a daughter board built with the same pin out as those LED arrays that could be swapped in.

     

    The key reason to swap to a micro-controller would be if you want to experiment with different algorithms for converting the movement to lights on.

     

    Could you do this with a nano, possibly, alternatively a Pro Mini or similar to get a few extra pins. You might need to use transistors to drive the LEDs, the ULN2003 is cheap and commonly available. You don't actually need a whole Arduino board to do this simply start with an ATMEGA328-PU chip. However, once you start making custom PCBs and putting a few other components on and you'll likely find yourself back in the $70 mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 10 years ago in reply to Former Member

    Hi Brian, it looks like you've got the bar graph chip Doug mentioned. If it is to go on a bike then I'd swap out those sockets and solder the chips directly but if it's to be office based then that's not an issue.

     

    To be honest $70 for a a small batch of boards is not a bad price. You will find that the costs are not due to the selection / number of components but the design and assembly time. If you have thousands to make then you should be able to get the unit cost down. I'd have thought you could swap the LED array out with high brightness LEDs, either thru hole or surface mounted to solve the light problem and reduce the part costs. If you can't change the board then you could have a daughter board built with the same pin out as those LED arrays that could be swapped in.

     

    The key reason to swap to a micro-controller would be if you want to experiment with different algorithms for converting the movement to lights on.

     

    Could you do this with a nano, possibly, alternatively a Pro Mini or similar to get a few extra pins. You might need to use transistors to drive the LEDs, the ULN2003 is cheap and commonly available. You don't actually need a whole Arduino board to do this simply start with an ATMEGA328-PU chip. However, once you start making custom PCBs and putting a few other components on and you'll likely find yourself back in the $70 mark.