Arduino Forum Temperature controlled relay (help needed for noobie)
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
  • Replies 17 replies
  • Subscribers 405 subscribers
  • Views 1097 views
  • Users 0 members are here
  • temperature
  • arduino
  • relay
Related

Temperature controlled relay (help needed for noobie)

Former Member
Former Member over 10 years ago

Hello, my name is Aisha this is my first post and I am excited to get into the community.


I live in a studio apartment with my wife. The entire apartment is on a 15amp breaker so we have to be careful about power use. We find if we run the A/C and cook something in the kitchen the fridge will kick on more often and trip our breaker. We have a blower to pull hot air out of the kitchen and I would like to use an arduino to turn it off and on based on the temperature.


I have:

 

an arduino uno

a tmp36 temperature sensor

a 5v arduino relay module

a breadboard and leads

 

I want to do this not only the right way and the best way with what I have available. I have used the arduino to switch the relay using the blinking LED code from a kit I got. I have wired up the sensor and read readings off of it.

 

 

The tutorials I find online say I should connect it to 3.3v and also AREF to 3.3v when I do this I don't get 3.3v in my serial monitor like the tutorials say but 1.5 (average). I am left lost as no tutorials show how to do this without an LCD screen and with a relay module. I don't need to monitor the temperature after I have it set properly once so an LCD is unnecessary (though I would not mind being able to add on in the future.)

 

I plan to put the sensor on a cable, are there limits to how long a cable can be for this sensor? I was planning on using cat5 cable.

 

So far all of my experiments with arduino involve copy pasting code and maybe modifying a couple lines that are clearly labeled or that a tutorial has told me to edit. I have 0% skills and about as much understanding and confidence in coding anything let alone a micro controller.

 

I have seen people adding things like data logging to increase accuracy of readings and delays to keep the switch from tripping like crazy but again I'm still struggling with the hardware and code is not at my level yet.

 

Hopefully there are people who can help me out. I know this is super easy for anyone who knows how to use and code arduino, I just need some help getting my first project finished.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +4
    aishalove First off, programming is not "super easy" as you say. I have done this most of my life and the biggest headache is to fix broken code. Even I break and fix my own code. I suggest read some about…
  • neilk
    neilk over 10 years ago +3
    aishalove Clem and Enrico have given you sound advice . For what it's worth, I have 2 basic rules when I am developing a project: Start small with something that should work - an example from the Arduino…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    What had not been said yet is the issue of driving mains with an arduino relay board. They are not all created to handle mains . Even if the physical elay is capable. The board may not be and mistakes…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    What had not been said yet is the issue of driving mains with an arduino relay board.

     

    They are not all created to handle mains . Even if the physical elay is capable. The board may not be and mistakes with mains can be rather unforgiving

     

    Don't know you expertise with mains control but if not much then seek advise here before you attempt it

     

    You can of course go right ahead and drive the relay board from the ardiino , just don't connect mains unless your sure.

     

    Many of these boards are designed for only 24v but still have 240v relays on them. So don't think is still safe just because the relay says so

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes Good point, Peter. I was suckered into buying such a relay board ( such a pretty blue colour; matches the Arduino!! ) early on in my Arduino experiments - I haven't used it to switch 240V !

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilk
    neilk over 10 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes Good point, Peter. I was suckered into buying such a relay board ( such a pretty blue colour; matches the Arduino!! ) early on in my Arduino experiments - I haven't used it to switch 240V !

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 10 years ago in reply to neilk

    I haven't used it to switch 240V !

    I would suggest using a Solid State Relay when it comes to 230v.

     

    The advantage is that some include a LED on the input side, and take no more energy that a LED.

     

    aishalove

     

    I found these two links for temperature controlling a relay.

    http://www.electroschematics.com/8998/arduino-temperature-controlled-relay/

    Make Your Own Temperature Controller with an Arduino

     

    They should help you with the code.

    I do have a sketch using DS18B20 One wire temperature sensor if you want to swap measuring devices.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to mcb1

    mcb1 Mark - I particularly like the one which uses the Maplin remote control power socket - Note, others types are available!

     

    It has the clear advantage of eliminating ANY need to work with mains voltages - it's all been done for you and is all neatly locked away.

     

    I already use some of these remote control power sockets, with their original control, to obviate the need to crawl under my desk to switch off my PC etc

    Very very useful at my age!

     

    Neil