Arduino Forum Analog pin value keep fluctuating in Arduino
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
  • Replies 10 replies
  • Subscribers 404 subscribers
  • Views 2788 views
  • Users 0 members are here
  • switch
  • arduino
Related

Analog pin value keep fluctuating in Arduino

Former Member
Former Member over 10 years ago

I  tried reading analog input for a switch.But the analog value is moving gradually from 0 to 1023 and back to 0 ,eventhough the switch is not pressed.

When switch is pressed,it reaches 1023.This is agreeable.

But when switch is not pressed,it reaches 1023.Please help me to resolve the issue.This will solve my other issue automatically...

I am using 20K ohm resistor.


#include <SPI.h>

#include <PubSubClient.h>

#include <Ethernet.h>

#include <util.h>

#include <ctype.h>

 

 

#define CLIENTID "ArduinoSensor"

#define TOPICNAME "switch/signal"

#define POLLINTERVAL 120000

 

#define PORT 80

//Connect to MQTT server

byte server1 [] = { X};

byte mac[] = {X};

 

IPAddress arduinoIP(X);

IPAddress dnsIP(X);

IPAddress gatewayIP(X);

IPAddress subnetIP(X);

EthernetServer server(PORT);

 

EthernetClient ethClient;

PubSubClient arduinoClient(server1, 8081, callback, ethClient);

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

 

 

int analogPin = 0;     // potentiometer wiper (middle terminal) connected to analog pin 3

 

                       // outside leads to ground and +5V

 

int val = 0;           // variable to store the value read

 

 

 

void setup()

 

{

 

  Serial.begin(9600);          //  setup serial

 

Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);

beginConnection() ;

}

 

void beginConnection() {

Serial.begin(9600);

//Ethernet.begin(mac) ;

int connRC = arduinoClient.connect(CLIENTID) ;

if (!connRC) {

Serial.println(connRC) ;

Serial.println("Could not connect to MQTT Server");

Serial.println("Please reset the arduino to try again");

delay(100);

exit(-1);

}

else {

Serial.println("Connected to MQTT Server...");

 

 

}}

 

void loop()

 

{

 

val = analogRead(analogPin);    // read the input pin

  Serial.println(val);
delay(100);  // debug value
if(val == 1023)
{
Serial.println("Button pressed and message published");
arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;

}

}

 

Its working better...But I see a problem with the analogRead...

The readings goes as below,

0

0

0

0

19

20

49

71

117

126

227

322

451

571

702

809

923

1023

Button pressed and message published

1023

Button pressed and message published

1023

Button pressed and message published

1022

1003

966

929

905

842

748

615

480

356

229

122

1

0

0

0

0

0

0

 

The readings gradually increasing till 1023 and then decreasing gradually.This should not happen as it is publishing messages when it is reaching 1023 without even pressing the switch.

But When the switch is pressed,it reaches 1023 and publishing the message.This is fine as this is required scenario..

 

Can you please help how to control the flow of analogRead?If this is kept under control,then my problem would be resolved...

  • Sign in to reply
  • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago

    Hello,

     

    I think that the reason of the fluctuation is just the switch. When you press the switch, the analog input receives a value, that is the highest and you see that it decreases if you put a resistor in series. Instead when the switch is not pressed, the analog input does not receives signals and - exactly as we can expect, the internal DA converter fluctuates. You get the same result if you try to read another analog pin with nothing connected.

     

    If you need read a switch on / off from the analog pin, I suggest to send the Vref to both the switch sides but to one of the two (e.g. the off position) you can put a resistor, e.g. 5K or more. So, then the switch is off, you receive a fixed value while then the switch is pressed the resistor is bypassed and you receive the highest value (1023, that you can assume it is the digital "1")

     

    Just a note: as you write you are already using a 20K resistor it is better if you put the scheme so it is possible to have an idea of what should be expected.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    Hi Enrico,

    Thanks for your reply..

    I am not from Electronics background...I could not understand the setup you have mentioned for noise reduction..

    Could you please show in circuit diagram or in anyother format so that I can buy necessary components and try the configuration..?

     

    Thanks,

    Radha

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member

    Hello,

     

    what I have asked is the circuit that you have done. Please put the drawing of the circuit so I figure out what you are doing. Else it is almost impossible.

     

    Thank you. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Former Member

    generk4

         Hello, there is a problem of reading a switch which should have a value of high or low with analog which is like a variable resistor. If the values are changing, you do not have the leg of the switch pulled to ground. In other words the switch is floating. You claimed it is 20K. Here is code and a picture of connecting a switch from arduino.cc:

     

    Code

    /* switch

    *

    * Each time the input pin goes from LOW to HIGH (e.g. because of a push-button

    * press), the output pin is toggled from LOW to HIGH or HIGH to LOW. There's

    * a minimum delay between toggles to debounce the circuit (i.e. to ignore

    * noise). 

    *

    * David A. Mellis

    * 21 November 2006

    */

    int inPin = 2;      // the number of the input pin

    int outPin = 13; // the number of the output pi

     

    int state = HIGH; // the current state of the output pin

    int reading; // the current reading from the input pin

    int previous = LOW; // the previous reading from the input pin

     

    // the follow variables are long's because the time, measured in milliseconds

    // will quickly become a bigger number than can be stored in an int.

    long time = 0;                   // the last time the output pin was toggled

    long debounce = 200;      // the debounce time, increase if the output flickers

     

    void setup()

    {

      pinMode(inPin, INPUT);

      pinMode(outPin, OUTPUT);

    }

     

    void loop()

    {

         reading = digitalRead(inPin);

     

      // if the input just went from LOW and HIGH and we've waited long enough

      // to ignore any noise on the circuit, toggle the output pin and remember

      // the time

      if (reading == HIGH && previous == LOW && millis() - time > debounce) {

        if (state == HIGH)

          state = LOW;

        else

          state = HIGH;

     

        time = millis(); 

      }

      digitalWrite(outPin, state);

     

      previous = reading;

    }

     

    PushButton.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    Hi Enrico,

    This is what I have done for the analog input,

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to clem57

    Thanks Clem.You have given me digital input code.I will try and update the status..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 10 years ago in reply to Former Member

    This looks wired incorrect.  The Analog line while the button is open, is floating unless you are using a internal pull up resistor.  The schematic should be like this.    Your Analog line is HELD high until you push the button. I did not change the resistor value, but 10K will work just fine.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to clem57

    Hi Clem Martins,

    Its working very fine image I am very happy image

    Thanks a lot for your help image

     

    Here is my MQTT program modified on your program

    #include <SPI.h>
    #include <PubSubClient.h>
    #include <Ethernet.h>
    #include <util.h>
    #include <ctype.h>
    
    
    
    
    #define CLIENTID "ArduinoSensor"
    #define TOPICNAME "switch/signal"
    #define POLLINTERVAL 120000
    
    
    #define PORT 80
    //Connect to MQTT server
    byte server1 [] = {192, 168, 1, 4};
    byte mac[] = {0x5e, 0xa4, 0x18, 0xf0, 0x8a, 0xf6};
    
    
    IPAddress arduinoIP(192, 168, 1, 67);
    IPAddress dnsIP(203, 145, 184, 32); 
    IPAddress gatewayIP(192, 168, 1, 1);
    IPAddress subnetIP(255, 255, 255, 0);
    EthernetServer server(PORT);
    
    
    EthernetClient ethClient;
    PubSubClient arduinoClient(server1, 8081, callback, ethClient);
    void callback(char* topic, byte* payload, unsigned int length) {
      // handle message arrived
    }
    int inPin = 2;      // the number of the input pin
    int outPin = 7; // the number of the output pi
    
    int state = HIGH; // the current state of the output pin
    int reading; // the current reading from the input pin
    int previous = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time = 0;                   // the last time the output pin was toggled
    long debounce = 200;      // the debounce time, increase if the output flickers
    
    void setup()
    {
      Serial.begin(9600);
      Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);
      pinMode(inPin, INPUT);
      pinMode(outPin, OUTPUT);
      beginConnection() ;
    }
    
     void beginConnection() {
    Serial.begin(9600);
    //Ethernet.begin(mac) ;
    int connRC = arduinoClient.connect(CLIENTID) ;
    if (!connRC) {
    Serial.println(connRC) ;
    Serial.println("Could not connect to MQTT Server");
    Serial.println("Please reset the arduino to try again");
    delay(100);
    exit(-1);
    }
    else {
    Serial.println("Connected to MQTT Server...");
    
    
    
    
    }}
    
    
    void loop()
    {
    
         reading = digitalRead(inPin);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading == HIGH && previous == LOW && millis() - time > debounce) {
        if (state == HIGH){
          state = LOW;
            arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");
        }
        else
        {
          state = HIGH;
          arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
           Serial.println("Button A is Pressed and message published");
        }
        time = millis(); 
      }
      digitalWrite(outPin, state);
      
      previous = reading;
    
    
    }

     

    Serial Port output is,

    Connected to MQTT Server...

    Button A is Pressed and message published

    Button A is Pressed and message published

    Button A is Pressed and message published

    Button A is Pressed and message published

    Button A is Pressed and message published

     

    This message is coming only when the switch is pressed.Also,MQTT is publishing only when the switch is pressed..image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    Now..I am going to connect two switches and want to produce result like,

    When Switch1 is pressed,it has to display "Switch1 is pressed".

    When switch2 is pressed,it has to display "Switch2 is pressed".

     

    I want to use digital pin only as what Clem given(below pic.) works fine for me...As I am not from Electronics background,can anyone help me to extend this for 2 to 3 switches please?

    PushButton.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    I tried to extend the same circuit with two switches and with the code below.Its working like charm image

    I am really thankful to Clem Martins...Thanks a lot for your help !image

    #include <SPI.h>
    #include <PubSubClient.h>
    #include <Ethernet.h>
    #include <util.h>
    #include <ctype.h>
    
    #define CLIENTID "ArduinoSensor"
    #define TOPICNAME "switch/signal"
    #define POLLINTERVAL 120000
    
    
    #define PORT 80
    //Connect to MQTT server
    byte server1 [] = {192, 168, 1, 4};
    byte mac[] = {0x5e, 0xa4, 0x18, 0xf0, 0x8a, 0xf6};
    
    
    IPAddress arduinoIP(192, 168, 1, 67);
    IPAddress dnsIP(203, 145, 184, 32); 
    IPAddress gatewayIP(192, 168, 1, 1);
    IPAddress subnetIP(255, 255, 255, 0);
    EthernetServer server(PORT);
    
    
    EthernetClient ethClient;
    PubSubClient arduinoClient(server1, 8081, callback, ethClient);
    void callback(char* topic, byte* payload, unsigned int length) {
      // handle message arrived
    }
    int inPin1 = 2; 
    int inPin2 = 0;// the number of the input pin
    int outPin = 7; // the number of the output pi
    
    int state = HIGH; // the current state of the output pin
    int reading; // the current reading from the input pin
    int previous = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time = 0;                   // the last time the output pin was toggled
    long debounce = 200;      // the debounce time, increase if the output flickers
    
    
    int state2 = HIGH; // the current state of the output pin
    int reading2; // the current reading from the input pin
    int previous2 = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time2 = 0;                   // the last time the output pin was toggled
    long debounce2 = 200;      // the debounce time, increase if the output flickers
    void setup()
    {
      Serial.begin(9600);
      Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);
        pinMode(inPin1, INPUT);
      pinMode(inPin2, INPUT);
      pinMode(outPin, OUTPUT);
      beginConnection() ;
    }
    
     void beginConnection() {
    Serial.begin(9600);
    //Ethernet.begin(mac) ;
    int connRC = arduinoClient.connect(CLIENTID) ;
    if (!connRC) {
    Serial.println(connRC) ;
    Serial.println("Could not connect to MQTT Server");
    Serial.println("Please reset the arduino to try again");
    delay(100);
    exit(-1);
    }
    else {
    Serial.println("Connected to MQTT Server...");
    
    
    
    
    }}
    
    
    void loop()
    {
    
        reading = digitalRead(inPin1);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading == HIGH && previous == LOW && millis() - time > debounce) {
        if (state == HIGH){
          state = LOW;
            arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");}
        else
        {
          state = HIGH;
             arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");
        }
        time = millis(); 
      }
      digitalWrite(outPin, state);
      
      previous = reading;
      
       reading2 = digitalRead(inPin2);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading2 == HIGH && previous2 == LOW && millis() - time2 > debounce2) {
        if (state2 == HIGH){
          state2 = LOW;
            arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");}
        else
        {
          state2 = HIGH;
          arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");
        }
        time2 = millis(); 
      }
      digitalWrite(outPin, state2);
      
      previous2 = reading2;
        
     }