Arduino Forum Analog pin value keep fluctuating in Arduino
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
  • Replies 10 replies
  • Subscribers 393 subscribers
  • Views 2592 views
  • Users 0 members are here
  • switch
  • arduino
Related

Analog pin value keep fluctuating in Arduino

Former Member
Former Member over 10 years ago

I  tried reading analog input for a switch.But the analog value is moving gradually from 0 to 1023 and back to 0 ,eventhough the switch is not pressed.

When switch is pressed,it reaches 1023.This is agreeable.

But when switch is not pressed,it reaches 1023.Please help me to resolve the issue.This will solve my other issue automatically...

I am using 20K ohm resistor.


#include <SPI.h>

#include <PubSubClient.h>

#include <Ethernet.h>

#include <util.h>

#include <ctype.h>

 

 

#define CLIENTID "ArduinoSensor"

#define TOPICNAME "switch/signal"

#define POLLINTERVAL 120000

 

#define PORT 80

//Connect to MQTT server

byte server1 [] = { X};

byte mac[] = {X};

 

IPAddress arduinoIP(X);

IPAddress dnsIP(X);

IPAddress gatewayIP(X);

IPAddress subnetIP(X);

EthernetServer server(PORT);

 

EthernetClient ethClient;

PubSubClient arduinoClient(server1, 8081, callback, ethClient);

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

 

 

int analogPin = 0;     // potentiometer wiper (middle terminal) connected to analog pin 3

 

                       // outside leads to ground and +5V

 

int val = 0;           // variable to store the value read

 

 

 

void setup()

 

{

 

  Serial.begin(9600);          //  setup serial

 

Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);

beginConnection() ;

}

 

void beginConnection() {

Serial.begin(9600);

//Ethernet.begin(mac) ;

int connRC = arduinoClient.connect(CLIENTID) ;

if (!connRC) {

Serial.println(connRC) ;

Serial.println("Could not connect to MQTT Server");

Serial.println("Please reset the arduino to try again");

delay(100);

exit(-1);

}

else {

Serial.println("Connected to MQTT Server...");

 

 

}}

 

void loop()

 

{

 

val = analogRead(analogPin);    // read the input pin

  Serial.println(val);
delay(100);  // debug value
if(val == 1023)
{
Serial.println("Button pressed and message published");
arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;

}

}

 

Its working better...But I see a problem with the analogRead...

The readings goes as below,

0

0

0

0

19

20

49

71

117

126

227

322

451

571

702

809

923

1023

Button pressed and message published

1023

Button pressed and message published

1023

Button pressed and message published

1022

1003

966

929

905

842

748

615

480

356

229

122

1

0

0

0

0

0

0

 

The readings gradually increasing till 1023 and then decreasing gradually.This should not happen as it is publishing messages when it is reaching 1023 without even pressing the switch.

But When the switch is pressed,it reaches 1023 and publishing the message.This is fine as this is required scenario..

 

Can you please help how to control the flow of analogRead?If this is kept under control,then my problem would be resolved...

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    Now..I am going to connect two switches and want to produce result like,

    When Switch1 is pressed,it has to display "Switch1 is pressed".

    When switch2 is pressed,it has to display "Switch2 is pressed".

     

    I want to use digital pin only as what Clem given(below pic.) works fine for me...As I am not from Electronics background,can anyone help me to extend this for 2 to 3 switches please?

    PushButton.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    I tried to extend the same circuit with two switches and with the code below.Its working like charm image

    I am really thankful to Clem Martins...Thanks a lot for your help !image

    #include <SPI.h>
    #include <PubSubClient.h>
    #include <Ethernet.h>
    #include <util.h>
    #include <ctype.h>
    
    #define CLIENTID "ArduinoSensor"
    #define TOPICNAME "switch/signal"
    #define POLLINTERVAL 120000
    
    
    #define PORT 80
    //Connect to MQTT server
    byte server1 [] = {192, 168, 1, 4};
    byte mac[] = {0x5e, 0xa4, 0x18, 0xf0, 0x8a, 0xf6};
    
    
    IPAddress arduinoIP(192, 168, 1, 67);
    IPAddress dnsIP(203, 145, 184, 32); 
    IPAddress gatewayIP(192, 168, 1, 1);
    IPAddress subnetIP(255, 255, 255, 0);
    EthernetServer server(PORT);
    
    
    EthernetClient ethClient;
    PubSubClient arduinoClient(server1, 8081, callback, ethClient);
    void callback(char* topic, byte* payload, unsigned int length) {
      // handle message arrived
    }
    int inPin1 = 2; 
    int inPin2 = 0;// the number of the input pin
    int outPin = 7; // the number of the output pi
    
    int state = HIGH; // the current state of the output pin
    int reading; // the current reading from the input pin
    int previous = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time = 0;                   // the last time the output pin was toggled
    long debounce = 200;      // the debounce time, increase if the output flickers
    
    
    int state2 = HIGH; // the current state of the output pin
    int reading2; // the current reading from the input pin
    int previous2 = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time2 = 0;                   // the last time the output pin was toggled
    long debounce2 = 200;      // the debounce time, increase if the output flickers
    void setup()
    {
      Serial.begin(9600);
      Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);
        pinMode(inPin1, INPUT);
      pinMode(inPin2, INPUT);
      pinMode(outPin, OUTPUT);
      beginConnection() ;
    }
    
     void beginConnection() {
    Serial.begin(9600);
    //Ethernet.begin(mac) ;
    int connRC = arduinoClient.connect(CLIENTID) ;
    if (!connRC) {
    Serial.println(connRC) ;
    Serial.println("Could not connect to MQTT Server");
    Serial.println("Please reset the arduino to try again");
    delay(100);
    exit(-1);
    }
    else {
    Serial.println("Connected to MQTT Server...");
    
    
    
    
    }}
    
    
    void loop()
    {
    
        reading = digitalRead(inPin1);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading == HIGH && previous == LOW && millis() - time > debounce) {
        if (state == HIGH){
          state = LOW;
            arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");}
        else
        {
          state = HIGH;
             arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");
        }
        time = millis(); 
      }
      digitalWrite(outPin, state);
      
      previous = reading;
      
       reading2 = digitalRead(inPin2);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading2 == HIGH && previous2 == LOW && millis() - time2 > debounce2) {
        if (state2 == HIGH){
          state2 = LOW;
            arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");}
        else
        {
          state2 = HIGH;
          arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");
        }
        time2 = millis(); 
      }
      digitalWrite(outPin, state2);
      
      previous2 = reading2;
        
     }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    I tried to extend the same circuit with two switches and with the code below.Its working like charm image

    I am really thankful to Clem Martins...Thanks a lot for your help !image

    #include <SPI.h>
    #include <PubSubClient.h>
    #include <Ethernet.h>
    #include <util.h>
    #include <ctype.h>
    
    #define CLIENTID "ArduinoSensor"
    #define TOPICNAME "switch/signal"
    #define POLLINTERVAL 120000
    
    
    #define PORT 80
    //Connect to MQTT server
    byte server1 [] = {192, 168, 1, 4};
    byte mac[] = {0x5e, 0xa4, 0x18, 0xf0, 0x8a, 0xf6};
    
    
    IPAddress arduinoIP(192, 168, 1, 67);
    IPAddress dnsIP(203, 145, 184, 32); 
    IPAddress gatewayIP(192, 168, 1, 1);
    IPAddress subnetIP(255, 255, 255, 0);
    EthernetServer server(PORT);
    
    
    EthernetClient ethClient;
    PubSubClient arduinoClient(server1, 8081, callback, ethClient);
    void callback(char* topic, byte* payload, unsigned int length) {
      // handle message arrived
    }
    int inPin1 = 2; 
    int inPin2 = 0;// the number of the input pin
    int outPin = 7; // the number of the output pi
    
    int state = HIGH; // the current state of the output pin
    int reading; // the current reading from the input pin
    int previous = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time = 0;                   // the last time the output pin was toggled
    long debounce = 200;      // the debounce time, increase if the output flickers
    
    
    int state2 = HIGH; // the current state of the output pin
    int reading2; // the current reading from the input pin
    int previous2 = LOW; // the previous reading from the input pin
    
    // the follow variables are long's because the time, measured in milliseconds
    // will quickly become a bigger number than can be stored in an int.
    long time2 = 0;                   // the last time the output pin was toggled
    long debounce2 = 200;      // the debounce time, increase if the output flickers
    void setup()
    {
      Serial.begin(9600);
      Ethernet.begin(mac, arduinoIP, dnsIP, gatewayIP, subnetIP);
        pinMode(inPin1, INPUT);
      pinMode(inPin2, INPUT);
      pinMode(outPin, OUTPUT);
      beginConnection() ;
    }
    
     void beginConnection() {
    Serial.begin(9600);
    //Ethernet.begin(mac) ;
    int connRC = arduinoClient.connect(CLIENTID) ;
    if (!connRC) {
    Serial.println(connRC) ;
    Serial.println("Could not connect to MQTT Server");
    Serial.println("Please reset the arduino to try again");
    delay(100);
    exit(-1);
    }
    else {
    Serial.println("Connected to MQTT Server...");
    
    
    
    
    }}
    
    
    void loop()
    {
    
        reading = digitalRead(inPin1);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading == HIGH && previous == LOW && millis() - time > debounce) {
        if (state == HIGH){
          state = LOW;
            arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");}
        else
        {
          state = HIGH;
             arduinoClient.publish(TOPICNAME, "Button A is Pressed") ;
          Serial.println("Button A is Pressed and message published");
        }
        time = millis(); 
      }
      digitalWrite(outPin, state);
      
      previous = reading;
      
       reading2 = digitalRead(inPin2);
    
      // if the input just went from LOW and HIGH and we've waited long enough
      // to ignore any noise on the circuit, toggle the output pin and remember
      // the time
      if (reading2 == HIGH && previous2 == LOW && millis() - time2 > debounce2) {
        if (state2 == HIGH){
          state2 = LOW;
            arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");}
        else
        {
          state2 = HIGH;
          arduinoClient.publish(TOPICNAME, "Button B is Pressed") ;
          Serial.println("Button B is Pressed and message published");
        }
        time2 = millis(); 
      }
      digitalWrite(outPin, state2);
      
      previous2 = reading2;
        
     }