Arduino Forum Arduino using Visual Studio
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
  • Replies 29 replies
  • Subscribers 404 subscribers
  • Views 3012 views
  • Users 0 members are here
Related

Arduino using Visual Studio

Workshopshed
Workshopshed over 10 years ago

Here's a free training course from Microsoft about using Visual Studio with the Arduino

 

https://www.microsoftvirtualacademy.com/en-US/training-courses/programming-robotic-systems-with-visual-studio-8321/?prid…

 

I'm not sure of the licensing implications but there does seem to be a free download of Visual Studio Community edition

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Visual Studio is an excelent tool for creating AVR (Arduino and Native) applications for the ATMEGA328 chips etc. and it is free. Atmel provide a completly free version of it directly from their site and…
  • bobcroft
    bobcroft over 10 years ago +2
    Another brilliant piece of software for programming Arduino's and the various derivatives is Visual Micro. The basic version is free and runs under Atmel Studio (certainly version 6.2) or Visual Studio…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    I suggest not to use it There are other better ways and as usual MS arrives bad and later. Enrico
Parents
  • bobcroft
    bobcroft over 10 years ago

    Another brilliant piece of software for programming Arduino's and the various derivatives is Visual Micro.  The basic version is free and runs under Atmel Studio (certainly version 6.2) or Visual Studio.  microsoft Visual Studio community edition is free.  If you want the debugger package with Visual Micro then there is a charge but it is still extremely cheap for what it can do.  Visual Micro (VM) adds loads of functionality to the basic Arduino IDE like 'intelisense',  better code highlighting, trace where functions are used etc.  I am only a beginner in programming but VM makes like so much easier.  The code developed in VM is totally compatible with the native Arduino IDE and can be opened and run in that IDE if desired.

    Naturally increased functionality adds to the learning curve but it is easy to get started and there are some good tutorials on line.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobcroft
    bobcroft over 10 years ago

    Another brilliant piece of software for programming Arduino's and the various derivatives is Visual Micro.  The basic version is free and runs under Atmel Studio (certainly version 6.2) or Visual Studio.  microsoft Visual Studio community edition is free.  If you want the debugger package with Visual Micro then there is a charge but it is still extremely cheap for what it can do.  Visual Micro (VM) adds loads of functionality to the basic Arduino IDE like 'intelisense',  better code highlighting, trace where functions are used etc.  I am only a beginner in programming but VM makes like so much easier.  The code developed in VM is totally compatible with the native Arduino IDE and can be opened and run in that IDE if desired.

    Naturally increased functionality adds to the learning curve but it is easy to get started and there are some good tutorials on line.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • neilk
    neilk over 10 years ago in reply to bobcroft

    bobcroft - I've just installed it; trying to get started, but run out of time image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to neilk

    If you have no idea why, I suggest a technical description of the scenario where you are running it. And what do you have installed exactly (components, plugins etc.)

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to balearicdynamics

    balearicdynamics It's Ok, thanks Enrico image. I will have another try when I have more time to devote to it.

     

    Neil