Arduino Forum can i talk to multiple arduinos at the same time with another arduino, in a serial format?
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
  • State Verified Answer
  • Replies 28 replies
  • Answers 3 answers
  • Subscribers 405 subscribers
  • Views 3107 views
  • Users 0 members are here
Related

can i talk to multiple arduinos at the same time with another arduino, in a serial format?

Former Member
Former Member over 10 years ago

Hello all,

 

I am trying to talk to multiple (say 4) microcontrollers (Arduinos) at the same time. I was wondering if i can setup a serial connection, with a selection line that can detect the neighbor Arduino and enable the corresponding pin to start the serial communication between the two. something like this:image

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 10 years ago +2 suggested
    Karim, further to Peter's reply I have done something similar to what you want to do using RS485 modules bought cheaply from China / Hong Kong. (Have a look on www.yourduino.com for modules and very useful…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 verified
    There are several options and without complex switching, the standard TTL pins on D0 and D1 are off the table, at least for direct use I2C is an option, each arduino would have its own address assigned…
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes +1 suggested
    it is quite of a simple concept: you have multiple units that you can mix and match to pave the way for an assistive surface for tactile sensing, which is modular. so the units may be added/removed from…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    There are several options and without complex switching, the standard TTL pins on D0 and D1 are off the table, at least for direct use

     

    I2C is an option, each arduino would have its own address assigned and they could all talk to each other or have one assigned as a master and act as a relay

    SPI could work but as it is based on using chip selects, as the number of nodes increases, the complexity goes up with it (Rapidly)

    with the addition of a simple RS232 (TTL) to RS485 (Differential Drive) chip on each arduino, you could implement a custom protocol or an old but still very popular industrial control protocol called MODBUS https://en.wikipedia.org/wiki/Modbus, this is still a defacto standard with many PLCs and other control devices, has been around since 1979 and there are drivers for most microcontrollers including many for the arduino

     

    Modbus would allow upto 127 devices to be attached onto a single RS485 serial link, I am actually currently working on projects using this protocol and will be integrating many different types of devices as I go, All educational purposes though, not for a specefic product

     

    Hope this helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    There are several options and without complex switching, the standard TTL pins on D0 and D1 are off the table, at least for direct use

     

    I2C is an option, each arduino would have its own address assigned and they could all talk to each other or have one assigned as a master and act as a relay

    SPI could work but as it is based on using chip selects, as the number of nodes increases, the complexity goes up with it (Rapidly)

    with the addition of a simple RS232 (TTL) to RS485 (Differential Drive) chip on each arduino, you could implement a custom protocol or an old but still very popular industrial control protocol called MODBUS https://en.wikipedia.org/wiki/Modbus, this is still a defacto standard with many PLCs and other control devices, has been around since 1979 and there are drivers for most microcontrollers including many for the arduino

     

    Modbus would allow upto 127 devices to be attached onto a single RS485 serial link, I am actually currently working on projects using this protocol and will be integrating many different types of devices as I go, All educational purposes though, not for a specefic product

     

    Hope this helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer