Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum can i talk to multiple arduinos at the same time with another arduino, in a serial format?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 28 replies
  • Answers 3 answers
  • Subscribers 419 subscribers
  • Views 4329 views
  • Users 0 members are here
Related

can i talk to multiple arduinos at the same time with another arduino, in a serial format?

e14 Contributor
e14 Contributor over 11 years ago

Hello all,

 

I am trying to talk to multiple (say 4) microcontrollers (Arduinos) at the same time. I was wondering if i can setup a serial connection, with a selection line that can detect the neighbor Arduino and enable the corresponding pin to start the serial communication between the two. something like this:image

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +2 suggested
    Karim, further to Peter's reply I have done something similar to what you want to do using RS485 modules bought cheaply from China / Hong Kong. (Have a look on www.yourduino.com for modules and very useful…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1 verified
    There are several options and without complex switching, the standard TTL pins on D0 and D1 are off the table, at least for direct use I2C is an option, each arduino would have its own address assigned…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes +1 suggested
    it is quite of a simple concept: you have multiple units that you can mix and match to pave the way for an assistive surface for tactile sensing, which is modular. so the units may be added/removed from…
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    There are several options and without complex switching, the standard TTL pins on D0 and D1 are off the table, at least for direct use

     

    I2C is an option, each arduino would have its own address assigned and they could all talk to each other or have one assigned as a master and act as a relay

    SPI could work but as it is based on using chip selects, as the number of nodes increases, the complexity goes up with it (Rapidly)

    with the addition of a simple RS232 (TTL) to RS485 (Differential Drive) chip on each arduino, you could implement a custom protocol or an old but still very popular industrial control protocol called MODBUS https://en.wikipedia.org/wiki/Modbus, this is still a defacto standard with many PLCs and other control devices, has been around since 1979 and there are drivers for most microcontrollers including many for the arduino

     

    Modbus would allow upto 127 devices to be attached onto a single RS485 serial link, I am actually currently working on projects using this protocol and will be integrating many different types of devices as I go, All educational purposes though, not for a specefic product

     

    Hope this helps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • bobcroft
    0 bobcroft over 11 years ago

    Karim,  further to Peter's reply I have done something similar to what you want to do using RS485 modules bought cheaply from China / Hong Kong. (Have a look on www.yourduino.com for modules and very useful information)  These modules contain the necessary parts to correctly terminate the differential line drivers.  One of the advantages of RS485 is that it can be used to link Arduino's 100's of meter's apart. These modules are easily connected to the Arduino's using either the hardware serial ports or the software ports using softSerial.  There is an Arduino library called EasyTransfer, by using this library you can transmit your data and the address of the recipient Arduino.  All Arduino's on the system receive the transmitted data but only the one with the matching address responds to it.  The RS485 bus is bi-directional so each Arduino can both send and receive data. You can use your own custom protocol as to what information you send.  MODBUS is well supported but was much more than I needed.

     

    Hope this helps

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bobcroft

    thank you all.

    now someone from another department was suggesting the use of Soft Serial ports.

    Would anyone here know about this? I have been reading and I found out it is a software approach to creating serial comm with non-serial pins on Arduino. Here is a link:

    https://www.arduino.cc/en/Reference/softwareSerial

    https://www.arduino.cc/en/Tutorial/MultiSerialMega

    now considering that I have already obtained Arduino Micro, I was hoping to know if I can use some of the pins to essentially create 6 simultaneous serial connections? I found the following link for it:

    AltSoftSerial Library, for an extra serial port

    but there is nothing there for Arduino Micro. I was wondering, on Micro, which pins do I have permission to use for serial comm.?

    I very much appreciate your help in this matter.

    Regards,

    Karim.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    the micro should still run the software without an issue but im doubtful if you will get six to run at the same tme, I would think you will run out of memory, RAM etc very fast and have no time to do other things on the arduino

     

    I think you will find that an RS485 aproach or I2C will serve you better and save a ship load of wireing too

     

    another low cost approach would be to use ethernet adapters with each one ot the new and low cost ESP WIFI adapters. All easy to use and can expand way beyond 6 units

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    I agree with Peter.

     

    I have tried one time only just for curiosity in past and strongly discourage the use of the soft serial method for a good result. Especially in this case that you want to create some kind of network.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Before you make a decision on the kind of networking hardware you need a bit of detail on the spec:

     

    The important things are:

     

    bandwidth - how much data into and out of each data on the network

    latency - how long you are able to wait from the time  anode sends out a message to the time it receives a reply from another node

    topology - you have drawn a star network with a single master  - is this really what you want

    maximum number of network nodes

    hardware cost constraints

    software cost constraints

    distance between nodes

     

    unless you define these things you can't design a good solution

     

    If you can put up with low bandwidth (a few kbit/s per node,) short distances, latencies of a few mS but must have very low hardware cost then a star or parallel connected soft UART based approach will work. If the distances are short you don't need any additional hardware at all. (I've used a soft UART on an LCD display controller talking to another micro a few feet away (did use hardware buffering for EMC reasons) at 2400 baud - many 10s of thousands of them made and works fine but takes far more software effort than using  a hardware UART (we were using an old micro and it's real UARTs were all used for other things.))

     

    If you need long distances and/or 10kbit/s or more data rates  then you need to think about UARTs. The Arduino has a single UART so perhaps your cheapest mid performance option is a a parallel 2 wire bus, using driver chips if longer than  few metres distance between nodes. (See Peter's suggestion.)

     

    So, as is usually the case, provide a bit more information and you'll get much better help.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thank you Michael,

    Here is a topology, as per your suggestion, that could happen. So, I have tried to show that any form of connection may exist between and among Arduinos.

    image

    These units are going to be snapped (and stuck) together, so the distance is zero (d = 0).

    Communication involves constant transfer of sensor values.

    As long as within a few milli secnds, the delay is likely not a problem.

    There could be anything from 2 to 10 or 11 nodes in a network. Virtually there should not be a problem in adding more units (other than the increase in delay).

    Thanks,

    Karim.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    What is the maximum number of nodes connecting to a single Arduino ?

     

    If you thinking like a dice then 6 but if a flat plane then probably 4, one on each side

     

    I am assuming then this is going to be som ekind of educational toy / kit like lego bricks concept ? or like playing scrabble but with physical connections

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Peter, the max. number of nodes connected to a single one would be 6.

    so, i am thinking of a swarm of units (like a swarm of robots, or in my case a swarm of sensors).

    well it is a bio-medical (tactile sensing) collection of units.

    Please advise.

    Karim.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Are you going to mix and match sensors where you could have more than one of a specific type on the same node ?

     

    sensor nodes would not necessarly need a microcontroller, you can have a controller that you add sensors too and this could drastically simplify the design

     

    Sensors can be connected via SPI or even easier I2C

     

    leaving only controller to controller communications to be done over the serial and this would be far simpler design

     

    Perhaps if your willing, you can share a little more detail of what your trying to acheive, as currently we are somewhat uessing what would be best for you and this will not be the best way to get good help

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>