Arduino Forum Sending a signal over a pin
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 1253 views
  • Users 0 members are here
  • signals
Related

Sending a signal over a pin

rishi2628
rishi2628 over 10 years ago

Is there any function in atmel studio or arduino that would help me send an 8 bit signal oven the B0 pin of atmega328p?

  • Sign in to reply
  • Cancel

Top Replies

  • gihu
    gihu over 10 years ago +3
    Hi, Serial library only works on pins with dedicated UART, ie in the UNO digital pin 0 and 1. For sending serial data over other pins you can use the SoftwareSerial library, which emulates the hardware…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Is there a reason you specifically want to use B0 or will any pin do Have you also considered using the I2C bus as this will also send 8 bts at a time to a destination via a hardwre UART, just a different…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Hello Rishi, if you need to send 8 bit on a single pin as a matter of fact it is a serialised byte. One option is to use the hardware serial, with the limitation of pins 0 and 1 that are connected to the…
Parents
  • gihu
    0 gihu over 10 years ago

    Hi,

     

    Serial library only works on pins with dedicated UART, ie in the UNO digital pin 0 and 1.

    For sending serial data over other pins you can use the SoftwareSerial library, which emulates the hardware by software, and you can chose the digital pins to act as Rx and Tx.

     

    See this https://www.arduino.cc/en/Reference/softwareSerial.

     

    Hope that helps!!!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 10 years ago

    Hi,

     

    Serial library only works on pins with dedicated UART, ie in the UNO digital pin 0 and 1.

    For sending serial data over other pins you can use the SoftwareSerial library, which emulates the hardware by software, and you can chose the digital pins to act as Rx and Tx.

     

    See this https://www.arduino.cc/en/Reference/softwareSerial.

     

    Hope that helps!!!

    • Cancel
    • Vote Up +3 Vote Down