Arduino Forum Sending a signal over a pin
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 1251 views
  • Users 0 members are here
  • signals
Related

Sending a signal over a pin

rishi2628
rishi2628 over 10 years ago

Is there any function in atmel studio or arduino that would help me send an 8 bit signal oven the B0 pin of atmega328p?

  • Sign in to reply
  • Cancel

Top Replies

  • gihu
    gihu over 10 years ago +3
    Hi, Serial library only works on pins with dedicated UART, ie in the UNO digital pin 0 and 1. For sending serial data over other pins you can use the SoftwareSerial library, which emulates the hardware…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Is there a reason you specifically want to use B0 or will any pin do Have you also considered using the I2C bus as this will also send 8 bts at a time to a destination via a hardwre UART, just a different…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Hello Rishi, if you need to send 8 bit on a single pin as a matter of fact it is a serialised byte. One option is to use the hardware serial, with the limitation of pins 0 and 1 that are connected to the…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Is there a reason you specifically want to use B0 or will any pin do

     

    Have you also considered using the I2C bus as this will also send 8 bts at a time to a destination via a hardwre UART, just a different protocol thats all.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Is there a reason you specifically want to use B0 or will any pin do

     

    Have you also considered using the I2C bus as this will also send 8 bts at a time to a destination via a hardwre UART, just a different protocol thats all.

    • Cancel
    • Vote Up +3 Vote Down