Arduino Forum RTC combined with servo device
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
  • State Not Answered
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 2230 views
  • Users 0 members are here
  • Design
Related

RTC combined with servo device

Former Member
Former Member over 10 years ago

Hello,

I have a project and part of it involve an RTC clock and a servo. see attachment below.

I already built the circuit but I am completely lost with the sketch.

The objective of the project is :

After every 3 hours the servo automatically rotate 60 degrees.

Hope you could help me in the sketch.

Thanks in advance!

 

image

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Can you show us what you have so far Have your already tried getting the servo to work using the standard servo library, same question for the RTC What is the model of the servo, I would normally recommend…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member +1
    You can make it change at what ever interval you like and as far as you like within its limits just write the program based on what info I provided and then share your results, and we can help further…
Parents
  • jasminemparham
    0 jasminemparham over 8 years ago

    Robert Peter Oakes I am doing something similar and I just found out today that I should add an RTC because I do want my servo to function on set times of the day except instead of it would be 20 degrees then down -20 degrees at a set time of day. Originally I was going to convert all set hours into milli secs but that might mess up my order everyday for the hours i want it set on.Would you suggest getting the RTC too?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jasminemparham
    0 jasminemparham over 8 years ago

    Robert Peter Oakes I am doing something similar and I just found out today that I should add an RTC because I do want my servo to function on set times of the day except instead of it would be 20 degrees then down -20 degrees at a set time of day. Originally I was going to convert all set hours into milli secs but that might mess up my order everyday for the hours i want it set on.Would you suggest getting the RTC too?