Arduino Forum RTC combined with servo device
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
  • State Not Answered
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 2230 views
  • Users 0 members are here
  • Design
Related

RTC combined with servo device

Former Member
Former Member over 10 years ago

Hello,

I have a project and part of it involve an RTC clock and a servo. see attachment below.

I already built the circuit but I am completely lost with the sketch.

The objective of the project is :

After every 3 hours the servo automatically rotate 60 degrees.

Hope you could help me in the sketch.

Thanks in advance!

 

image

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Can you show us what you have so far Have your already tried getting the servo to work using the standard servo library, same question for the RTC What is the model of the servo, I would normally recommend…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member +1
    You can make it change at what ever interval you like and as far as you like within its limits just write the program based on what info I provided and then share your results, and we can help further…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Can you show us what you have so far

     

    Have your already tried getting the servo to work using the standard servo library, same question for the RTC

     

    What is the model of the servo, I would normally recommend NOT connecting the motors to the regulated output of the Arduino Power Supply as it invariably causes issues. Power it separately if you can

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    the servo is the MG996R and the rtc 1307:

     

     

    #include <Wire.h>

    #include "RTClib.h"

     

     

    RTC_DS1307 rtc;

     

     

    void setup () {

      Serial.begin(57600);

    #ifdef AVR

      Wire.begin();

    #else

      Wire1.begin(); // Shield I2C pins connect to alt I2C bus on Arduino Due

    #endif

      rtc.begin();

     

     

      if (! rtc.isrunning()) {

        Serial.println("RTC is NOT running!");

        // following line sets the RTC to the date & time this sketch was compiled

        rtc.adjust(DateTime(F(__DATE__), F(__TIME__)));

        // This line sets the RTC with an explicit date & time, for example to set

        // January 21, 2014 at 3am you would call:

        // rtc.adjust(DateTime(2014, 1, 21, 3, 0, 0));

      }

    }

     

     

    void loop () {

        DateTime now = rtc.now();

       

        Serial.print(now.year(), DEC);

        Serial.print('/');

        Serial.print(now.month(), DEC);

        Serial.print('/');

        Serial.print(now.day(), DEC);

        Serial.print(' ');

        Serial.print(now.hour(), DEC);

        Serial.print(':');

        Serial.print(now.minute(), DEC);

        Serial.print(':');

        Serial.print(now.second(), DEC);

        Serial.println();

       

        Serial.print(" since midnight 1/1/1970 = ");

        Serial.print(now.unixtime());

        Serial.print("s = ");

        Serial.print(now.unixtime() / 86400L);

        Serial.println("d");

       

        // calculate a date which is 7 days and 30 seconds into the future

        DateTime future (now.unixtime() + 7 * 86400L + 30);

       

        Serial.print(" now + 7d + 30s: ");

        Serial.print(future.year(), DEC);

        Serial.print('/');

        Serial.print(future.month(), DEC);

        Serial.print('/');

        Serial.print(future.day(), DEC);

        Serial.print(' ');

        Serial.print(future.hour(), DEC);

        Serial.print(':');

        Serial.print(future.minute(), DEC);

        Serial.print(':');

        Serial.print(future.second(), DEC);

        Serial.println();

       

        Serial.println();

        delay(3000);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    the servo is the MG996R and the rtc 1307:

     

     

    #include <Wire.h>

    #include "RTClib.h"

     

     

    RTC_DS1307 rtc;

     

     

    void setup () {

      Serial.begin(57600);

    #ifdef AVR

      Wire.begin();

    #else

      Wire1.begin(); // Shield I2C pins connect to alt I2C bus on Arduino Due

    #endif

      rtc.begin();

     

     

      if (! rtc.isrunning()) {

        Serial.println("RTC is NOT running!");

        // following line sets the RTC to the date & time this sketch was compiled

        rtc.adjust(DateTime(F(__DATE__), F(__TIME__)));

        // This line sets the RTC with an explicit date & time, for example to set

        // January 21, 2014 at 3am you would call:

        // rtc.adjust(DateTime(2014, 1, 21, 3, 0, 0));

      }

    }

     

     

    void loop () {

        DateTime now = rtc.now();

       

        Serial.print(now.year(), DEC);

        Serial.print('/');

        Serial.print(now.month(), DEC);

        Serial.print('/');

        Serial.print(now.day(), DEC);

        Serial.print(' ');

        Serial.print(now.hour(), DEC);

        Serial.print(':');

        Serial.print(now.minute(), DEC);

        Serial.print(':');

        Serial.print(now.second(), DEC);

        Serial.println();

       

        Serial.print(" since midnight 1/1/1970 = ");

        Serial.print(now.unixtime());

        Serial.print("s = ");

        Serial.print(now.unixtime() / 86400L);

        Serial.println("d");

       

        // calculate a date which is 7 days and 30 seconds into the future

        DateTime future (now.unixtime() + 7 * 86400L + 30);

       

        Serial.print(" now + 7d + 30s: ");

        Serial.print(future.year(), DEC);

        Serial.print('/');

        Serial.print(future.month(), DEC);

        Serial.print('/');

        Serial.print(future.day(), DEC);

        Serial.print(' ');

        Serial.print(future.hour(), DEC);

        Serial.print(':');

        Serial.print(future.minute(), DEC);

        Serial.print(':');

        Serial.print(future.second(), DEC);

        Serial.println();

       

        Serial.println();

        delay(3000);

    }