Arduino Forum NRF24L01 Problem simplifying code
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
  • State Verified Answer
  • Replies 16 replies
  • Answers 3 answers
  • Subscribers 404 subscribers
  • Views 2487 views
  • Users 0 members are here
  • nrf24l01
Related

NRF24L01 Problem simplifying code

billpenner
billpenner over 10 years ago

I am using the NRF24 for receiver/transmitter on a link between a Uno and a Mega. the basis for the code is http://maniacbug.github.io/RF24 I have finally gotten the units working super. My project is to input a four digit code on the transmitter, send it to the receiver, which will echo back the data sent for accuracy check. Then the code will be displayed on a  three inch 7 segment display. My problem is: The code from the above is impossible for me to modify without breaking it. It seems that most of the work is done in the library RF24.h. The code is great for debugging and was very helpful for getting the NRF24s working. However, All my efforts to simplify the code to insert the data and extract it results in compiler errors. Does anyone have any help or a source for a more easily modified code for the NRF24?

Thanks to a bunch of great resource and to the dedication to us who are trying to learn.

Bill

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago +2
    Hello Bill, Please can you put here the parts of code that you have in mind to break and simplify ? Maybe that there is some parts global that should be replaced in a different way. Thank you. Enrico
  • m.ratcliffe
    m.ratcliffe over 10 years ago +1
    The Blue link sends me back to this page, is the library you are using upto date? I got the following from: NRF24: NRF24 library for Arduino " This NRF24 library has now been superceded by the RadioHead…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    you may find the code here useful for reference, I used the NRF modules in last XMAS contest and provided all the code http://www.element14.com/community/groups/arduino/blog/2015/01/24/byob-party-15-news…
Parents
  • m.ratcliffe
    0 m.ratcliffe over 10 years ago

    The Blue link sends me back to this page, is the library you are using upto date?

     

    I got the following from: NRF24: NRF24 library for Arduino

     

    "This NRF24 library has now been superceded by the RadioHead library http://www.airspayce.com/mikem/arduino/RadioHead RadioHead and its RH_NRF24 driver provides all the features supported by NRF24, and much more besides, including Reliable Datagrams, Addressing, Routing and Meshes. All the platforms that NRF24 supported are also supported by RadioHead."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • m.ratcliffe
    0 m.ratcliffe over 10 years ago

    The Blue link sends me back to this page, is the library you are using upto date?

     

    I got the following from: NRF24: NRF24 library for Arduino

     

    "This NRF24 library has now been superceded by the RadioHead library http://www.airspayce.com/mikem/arduino/RadioHead RadioHead and its RH_NRF24 driver provides all the features supported by NRF24, and much more besides, including Reliable Datagrams, Addressing, Routing and Meshes. All the platforms that NRF24 supported are also supported by RadioHead."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billpenner
    0 billpenner over 10 years ago in reply to m.ratcliffe

    I'm sorry, the correct link is https://maniacbug.wordpress.com/2011/11/02/getting-started-rf24/#more-229.

    I don't why the other link sent you in a circle.

    I worked with the radiohead  for a long time but never got it working with Arduino Uno or Mega.

    thanks for the reply.