Arduino Forum Arduino as a FTDI chip
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 402 subscribers
  • Views 322 views
  • Users 0 members are here
  • to
  • arduino
  • ftdi
Related

Arduino as a FTDI chip

rishi2628
rishi2628 over 10 years ago

The thing is that i have an ESP8266 Wifi Module that can be programmed by an FTDI chip, which i dont have. I was wondering that whether i can use my arduino as a FTDI programmer. This is a picture of my arduino. I know that there are 2 avr microcontrollers on the board. One is used to convert USB signals to Tx Rx signals and the other gets programmed. Can i convert the first to an FTDI??

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    There are two Atmel chips on board, one is completly tied up with USB functionality and communicates with the ATMEGA328 using its only serial port (Hardware one) but you can use the software serial library…
  • binarygenius
    binarygenius over 10 years ago +1
    here you go mate there is a good instructable here on how to do it Arduino Examples #2 Use an Arduino as a FTDI Programmer and as Peter said you can use the arduino as a serial interface because that is…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    There are two Atmel chips on board, one is completly tied up with USB functionality and communicates with the ATMEGA328 using its only serial port (Hardware one) but you can use the software serial library and acheive the same thing, you would then write a sketch to copy everything comming in on the USB based serial out to the software serial and everything comming in on the software serial back up the USB based serial to the PC... done image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    There are two Atmel chips on board, one is completly tied up with USB functionality and communicates with the ATMEGA328 using its only serial port (Hardware one) but you can use the software serial library and acheive the same thing, you would then write a sketch to copy everything comming in on the USB based serial out to the software serial and everything comming in on the software serial back up the USB based serial to the PC... done image