Arduino Forum Shift registers. SPI or daisychain ?
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 403 subscribers
  • Views 644 views
  • Users 0 members are here
  • spi
  • shift_register
  • 74hc595
Related

Shift registers. SPI or daisychain ?

Former Member
Former Member over 10 years ago

Hi everybody. Please forgive me if that question have been asked before (i didn't find anything on this forum though).

 

I am planning to use shift registers (74HC595) to drive solenoids and I am wondering what is the difference between daisychaining the 595s ans using SPI

At same time I am wondering what is the point of using SPI since on the schematics I saw over the internet requires to link the 595s chips via their Serial input pins (like when daisychaining).

 

Would it be possible to use each 595s as a Slave without linking them each other (probably not since they don't have a chip select pin).

 

Any help / advice will be appreciated.

 

Have a good day/night.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    you could linkeach of those chips in series or have them seperate but that will require alot more pins of course A better option in my opinopn is the CD74HC4094 which can be directly connecte to a SPI…
  • Former Member
    Former Member over 10 years ago +1
    Thank you Peter and Enrico for your answers. I will have a look at theses ICs your mention. although I think I will go with 74hc595 daisychained since I have dozens of them already at hand.
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you could linkeach of those chips in series or have them seperate but that will require alot more pins of course

     

    A better option in my opinopn is the CD74HC4094 which can be directly connecte to a SPI bus and if you want each can have the strobe line to a different I/O or together if the chips are put in series.

     

    the other one which provides more flexability is the MCP23S17 which gives you 16 i/o lines all in one SPI attached chip

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you could linkeach of those chips in series or have them seperate but that will require alot more pins of course

     

    A better option in my opinopn is the CD74HC4094 which can be directly connecte to a SPI bus and if you want each can have the strobe line to a different I/O or together if the chips are put in series.

     

    the other one which provides more flexability is the MCP23S17 which gives you 16 i/o lines all in one SPI attached chip