Arduino Forum ARDUINO bitvoicer ir sending
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 400 views
  • Users 0 members are here
Related

ARDUINO bitvoicer ir sending

Former Member
Former Member over 9 years ago

hello

i've got problem with my program

im using arduino mega. when i use bit voicer and irremote the ir led is blink so slow that tv cannot get right signal to turn off. when i use only irremote everything is ok. So i thinking that bitvoicer is slowing down irremote or maybe my program is wrong. i tried different timer in irremote library but it isn't work.

can enyone help me in this??

 

 

CODE

 

#include <IRremote.h>

#include <IRremoteInt.h>

 

 

 

 

IRsend irsend;

 

#include <BitVoicer11.h>

//właczanie bita

BitVoicerSerial bvSerial = BitVoicerSerial();

byte dataType = 4;

int OutPutPins[] = {10,12,11,8};

int pinCount = 4;

int wl = 0 ;

void setup() {

  Serial.begin(115200);

  for(int activePin =0; activePin <pinCount; activePin++){

    pinMode(OutPutPins[activePin],OUTPUT);

  } 

   pinMode(7, OUTPUT);

   pinMode(9, OUTPUT);

   digitalWrite(7,HIGH);// put your setup code here, to run once:

pinMode(5,INPUT_PULLUP);

 

}

 

 

void loop() {

 

}

}

void serialEvent()

{

 

 

dataType = bvSerial.getData();

 

//Changes the value of sampleTest if the received data was

//the start/stop sampling command

if (dataType == BV_COMMAND)

 

 

//Signals BitVoicer's Speech Recognition Engine to start

//listening to audio streams after the engineRunning status

//was received

if (dataType == BV_STATUS && bvSerial.engineRunning == true)

   bvSerial.startStopListening();

 

 

if (dataType == BV_INT)

{

  int pinNumber = bvSerial.intData;

digitalWrite(pinNumber, !digitalRead(pinNumber));

delay(50);

}

// tutaj wartości string czyli pisane

if(dataType == BV_STR)

{

  if (bvSerial.strData == "okej")

  digitalWrite(7,LOW);

  delay(500);

digitalWrite(7,HIGH);

 

if (bvSerial.strData == "klas")

digitalWrite(9,HIGH);

delay(1);

 

if (bvSerial.strData == "klass")

digitalWrite(9,LOW);

 

if (bvSerial.strData == "komplet")

  irsend.sendNEC(0x5EA100FE, 32);

  delay(400);

  digitalWrite(7,LOW);

  delay(500);

  digitalWrite(7,HIGH);

  irsend.sendNEC(0x20DF10EF, 32);

 

if (bvSerial.strData == "wiez")

  irsend.sendNEC(0x7E8154AB, 32);

 

if (bvSerial.strData == "tv")

 

  irsend.sendNEC(0x20DF10EF, 32);

 

 

if (bvSerial.strData == "klim");

  irsend.sendNEC(0x8F758A7, 32);

 

if (bvSerial.strData == "h1")

irsend.sendNEC(0x5EA1E21C,32);

 

if (bvSerial.strData == "h2")

irsend.sendNEC(0x5EA152AC, 32);

 

if (bvSerial.strData == "h3")

irsend.sendNEC(0x5EA1B24C,32);

 

if (bvSerial.strData == "h4")

irsend.sendNEC(0x5EA10AF4,32);

 

if (bvSerial.strData == "mut")

irsend.sendNEC(0x5EA138C7,32);

 

if (bvSerial.strData == "rad")

irsend.sendNEC(0x5EA1609,32);

 

if (bvSerial.strData == "en")

irsend.sendNEC(0x5EA1C03E,32);

if (bvSerial.strData == "pc")

irsend.sendNEC(0x5EA100FE,32);

if (bvSerial.strData == "opt")

irsend.sendNEC(0x5EA1D628,32);

delay(400);

irsend.sendNEC(0x5EA1B946,32);

delay(400);

irsend.sendNEC(0x5EA17B84,32);

delay(400);

irsend.sendNEC(0x5EA17986,32);

delay(400);

irsend.sendNEC(0x5EA155AA,32);

delay(400);

irsend.sendNEC(0x5EA155AA,32);

 

if (bvSerial.strData == "hd")

irsend.sendNEC(0x5EA1D628,32);

delay(400);

irsend.sendNEC(0x5EA1B946,32);

delay(400);

irsend.sendNEC(0x5EA17B84,32);

delay(400);

irsend.sendNEC(0x5EA1F906,32);

delay(400);

irsend.sendNEC(0x5EA17B84,32);

delay(400);

irsend.sendNEC(0x5EA17B84,32);

if (bvSerial.strData == "opc")

irsend.sendNEC(0x5EA1D628,32);

if (bvSerial.strData == "cof")

irsend.sendNEC(0x5EA155AA,32);

delay(200);

irsend.sendNEC(0x20DF14EB,32);

if (bvSerial.strData == "wyj")

irsend.sendNEC(0x20DFDA25,32);

if (bvSerial.strData == "set")

irsend.sendNEC(0x5EA121DE,32);

if (bvSerial.strData == "ok")

irsend.sendNEC(0x5EA17B84,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "dir")

irsend.sendNEC(0x5EA1BB44,32);

if (bvSerial.strData == "pros")

irsend.sendNEC(0x5EA16A95,32);

if (bvSerial.strData == "cis")

irsend.sendNEC(0x5EA1D827,32);

 

if (bvSerial.strData == "dol")

irsend.sendNEC(0x5EA139C6,32);

delay(100);

irsend.sendNEC(0x20DF827D,32);

if (bvSerial.strData == "gora")

irsend.sendNEC(0x5EA1B946,32);

delay(100);

irsend.sendNEC(0x20DF02FD,32);

if (bvSerial.strData == "pr")

irsend.sendNEC(0x5EA17986,32);

delay(100);

irsend.sendNEC(0x20DF609F,32);

if (bvSerial.strData == "lew")

irsend.sendNEC(0x5EA1F906,32);

delay(100);

irsend.sendNEC(0x20DFE01F,32);

if (bvSerial.strData == "inp")

irsend.sendNEC(0x20DFD02F,32);

if (bvSerial.strData == "tel")

irsend.sendNEC(0x20DFD02F,32);

delay(100);

irsend.sendNEC(0x20DFD02F,32);

if (bvSerial.strData == "jeden")

irsend.sendNEC(0x20DFD02F,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "dwujka")

irsend.sendNEC(0x20DF48B7,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "trujka")

irsend.sendNEC(0x20DFC837,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "polsat")

irsend.sendNEC(0x20DF28D7,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "tvn")

irsend.sendNEC(0x20DFA85,32);

delay(100);

irsend.sendNEC(0x20DF22DD,32);

if (bvSerial.strData == "next")

irsend.sendNEC(0x20DF00FF,32);

 

if (bvSerial.strData == "prev")

irsend.sendNEC(0x20DF807F,32);

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +1 suggested
    Your code is hard to follow, because it is missing indentation. You can edit your post, and use the syntax highlighting tool in the editor on this website (Click on the icon that looks like '>>' and navigate…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1 verified
    Asside from the comments from Shabaz which I totally agree with, indentation and neat readable code is essential in helping with debuging there is one obvious thing wrong with your code if (bvSerial.strData…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Your code is hard to follow, because it is missing indentation.

    You can edit your post, and use the syntax highlighting tool in the editor on this website (Click on the icon that looks like '>>' and navigate down to

    Syntax Highlighting.

    Then you can show code that looks like this (example), with indentation - much easier to follow and troubleshoot/debug as you can see:

    #include stdio.h
    int
    main(void)
    {
     // code
     return(0);
    }

     

    Also, as a general hint, to get you moving forward, I'd advise cutting down your code until you are only performing actions for one command/IR signal.

    If you can get that to work, then you can scale to the larger program.

    If you can't get that smaller program to work, can you paste it with indentations so we can follow it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Your code is hard to follow, because it is missing indentation.

    You can edit your post, and use the syntax highlighting tool in the editor on this website (Click on the icon that looks like '>>' and navigate down to

    Syntax Highlighting.

    Then you can show code that looks like this (example), with indentation - much easier to follow and troubleshoot/debug as you can see:

    #include stdio.h
    int
    main(void)
    {
     // code
     return(0);
    }

     

    Also, as a general hint, to get you moving forward, I'd advise cutting down your code until you are only performing actions for one command/IR signal.

    If you can get that to work, then you can scale to the larger program.

    If you can't get that smaller program to work, can you paste it with indentations so we can follow it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer