Arduino
  • Products
  • More
Arduino
Arduino Forum Motors for Arduino and embedded PC projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 849 views
  • Users 0 members are here
  • motor
  • arduino
Related

Motors for Arduino and embedded PC projects

amrrahmy
amrrahmy over 10 years ago

I have read a bit about the differences between DC / servo / stepper motors, but I would like to know more before delving any deeper.

 

the projects will use

  • Arduino Uno (possibly Arduino Zero in the future or other ARM micro-controllers),
  • 5.3V 2A USB smartphone charger as the input

 

wanted to make a "pan / tilt"(possibly 360 degree) platform for a solar panel (3W or 5W + the weight or the platform (probably made of wood))

  • are there any pros or cons if I use a servo vs stepper motor(more components, more expensive, more power required, more accuracy)

 

wanted to make a lift(elevator) and pulley system that would lift and move maybe 1-2KG(2-4 pounds) across 1 meter distance(might add hydraulics if needed)

  • would a DC motor have more torque if I added gears or would I be better off looking for a servo motor(any additional electronics needed for either? transformers, more power required to do the same job, ...etc.)
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago in reply to amrrahmy +2 suggested
    Hi Amr, You can connect the hobby servo to an external supply yes, and connect the control wire to a digital output on the Arduino (a pulse width modulation or PWM signal is used, see here ). Motor drivers…
  • shabaz
    shabaz over 10 years ago +1 verified
    Hi Amr, There is a post here that highlights some differences between the various types of motors . There are example photos there too, so you can recognise the motors. A 3W/5W panel is fairly small, so…
Parents
  • bhavikbhansali
    0 bhavikbhansali over 10 years ago

    My suggestion for lift is use high torque (less RPM) gear motor and by using arduino's PWM pin you can control motor position as well as speed too. By doing this you will get accuracy in lift.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhavikbhansali
    0 bhavikbhansali over 10 years ago

    My suggestion for lift is use high torque (less RPM) gear motor and by using arduino's PWM pin you can control motor position as well as speed too. By doing this you will get accuracy in lift.