Arduino Forum Programming The Atmega2560 with Arduino
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
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 1644 views
  • Users 0 members are here
  • arduino_tutorials
  • arduino_tutorial
Related

Programming The Atmega2560 with Arduino

technocat
technocat over 9 years ago

Hi everyone,

 

I joined element14 because I recently started building a PCB on Eagle for an independent study for school, and I need some help.

 

I want to use the Atmega2560 board due to its large analog input, digital I/O capacity, and Arduino uses it in the Mega so the pinouts are simple. My only issue is that I can't find a way to program the board!

 

It seems that the Atmega2560 doesn't come with the Arduino bootloader installed (not surprising) and I can't find a pre-bootloaded board on the internet either, like some other Atmel boards.

 

My question really is:

 

How can I upload an Arduino sketch a stock Atmel ATMega2560 IC?

 

Thanks A LOT to anyone with information!

  • Sign in to reply
  • Cancel

Top Replies

  • technocat
    technocat over 9 years ago in reply to clem57 +2
    Hi Clem, I'm building a 10.5 foot drone that can take off vertically and fly horizontally. Its like the Osprey V-22. The hardware necessary to make that happen doesn't really exist beyond the commercial…
Parents
  • Former Member
    0 Former Member over 9 years ago

    The usual IDE for Atmel chips is Atmel Studio (currently version 7).  There are physical connections that have to be made with some type of link between a computer and the chip. 

     

    One of the least expensive options for a breadboarded chip is Freetronics USB adapter and the Arduino IDE.  You can break out the pins to serve as a programmer.  Up in price from there would be Atmel's programmers (AVR Dragon, for example), or a Segger (if you want the Cadillac programmer).

     

    Here's a link to the Atmel page on the AVR ATmega2560.  There are links to documentation and hardware that can be used with the chip:

    ATmega2560

     

    If you wanted to go with a low cost programmer here's a YouTube video that someone did on just that: https://www.youtube.com/watch?v=qT-d0di_Hq0

    You can also use AVRDude.  Another good site to pose your question is AVR Freaks ( www.avrfreaks.net ).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    The usual IDE for Atmel chips is Atmel Studio (currently version 7).  There are physical connections that have to be made with some type of link between a computer and the chip. 

     

    One of the least expensive options for a breadboarded chip is Freetronics USB adapter and the Arduino IDE.  You can break out the pins to serve as a programmer.  Up in price from there would be Atmel's programmers (AVR Dragon, for example), or a Segger (if you want the Cadillac programmer).

     

    Here's a link to the Atmel page on the AVR ATmega2560.  There are links to documentation and hardware that can be used with the chip:

    ATmega2560

     

    If you wanted to go with a low cost programmer here's a YouTube video that someone did on just that: https://www.youtube.com/watch?v=qT-d0di_Hq0

    You can also use AVRDude.  Another good site to pose your question is AVR Freaks ( www.avrfreaks.net ).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer