Arduino
  • Products
  • More
Arduino
Arduino Forum Parsing integer strings?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 410 subscribers
  • Views 2806 views
  • Users 0 members are here
  • serial_communications
  • potentiometers
  • parsing
  • boolean
  • arduino
Related

Parsing integer strings?

scorpion
scorpion over 10 years ago

I need help with parsing a string of integers sent from another Arduino. The values will be like this 1, 0, 1234, 1234,

1 is a Boolean

0 is a Boolean

1234 are pot values

I would like for it to go to variables

Vpot is first pot value

Hpot is second pot value

C is first Boolean

Z is second Boolean

 

Thanks,

Ben Bonen

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    sscanf is your friend, probably supported by Arduino (I don't use Arduino). Reddit on the topic however is here. https://www.reddit.com/r/arduino/comments/pznnj/using_sscanf_with_arduino/
  • gadget.iom
    gadget.iom over 10 years ago +1
    The Serial.readStringUntil command may help you if you are receiving the data through the serial port. Something like this might work: void loop(){ String C = Serial.readStringUntil(',').toInt(); Serial…
  • clem57
    clem57 over 10 years ago +1
    One way is using indexOf( ) like in http://stackoverflow.com/questions/11068450/arduino-c-language-parsing-string-with-delimiter-input-through-serial-interf… Then easy to convert to known values. Suggest…
  • shabaz
    0 shabaz over 10 years ago

    sscanf is your friend, probably supported by Arduino (I don't use Arduino). Reddit on the topic however is here.

    https://www.reddit.com/r/arduino/comments/pznnj/using_sscanf_with_arduino/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hi Ben,

     

    please find below the method I have used in several string parsers with the Arduino boards. This will work for sure.

     

    Enrico

     

    /** \fn int charsToInt(int startChar, int numChars)
        \brief Convert a string from the command to integer
    
    
        \param startChar initial character in the command string
        \param numChars number of characters composing the number
        \return The converted interger value
    */
    int charsToInt(int startChar, int numChars)
    {
        char * value_to_convert;
        String temp = String(6);
        int i;
    
    
        for (i = 0; i < numChars; i++)
            temp += cmd.cmdData[i + startChar];
    
    
        value_to_convert = temp;
        i = atoi(temp);
    
    
        return i;
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to balearicdynamics

    That might be a bit difficult to implement where the value of vpot falls below 1000.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago

    The Serial.readStringUntil command may help you if you are receiving the data through the serial port.

    Something like this might work:

    void loop(){
        String C  = Serial.readStringUntil(',').toInt();
        Serial.read(); //next character is a comma, so skip it using this
        String Z = Serial.readStringUntil(',').toInt();
        Serial.read();
        String Vpot = Serial.readStringUntil(',').toInt();
        Serial.read();
        String Hpot  = Serial.readStringUntil(',').toInt();
    }

     

    [This code is untested]

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    One way is using  indexOf( )  like in http://stackoverflow.com/questions/11068450/arduino-c-language-parsing-string-with-delimiter-input-through-serial-interf…

    Then easy to convert to known values. Suggest to check errors like invalid characters or ???

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    Second approach is download SDK at https://parse.com/docs/arduino/guide

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scorpion
    0 scorpion over 10 years ago in reply to balearicdynamics

    @Enrico Miglino

    Thanks!

    Will this send the values to different variables?

    Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to scorpion

    Hi Ben,

     

    as this is an independent function, you can call it passing the string you want to parse and use the integer return value as well. About the error correction it is true, there is no error checking and - by my point of view - there is a reason. As this function is used in a parser; I mean, a string parser processing multiple kind of commands with or without parameters, command separators etc. when the conversion is called all the syntax check are already done.

     

    In your case I suggest you check before that the string you send is a valid numeric string that - by a pragmatic point of view - is something independent by the conversion function. In this moment I don't remember what kind of result aoti() call returns when a non-numeric character is passed.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to gadget.iom

    Hi Paul,

     

    what do you mean with vpot ?

    (maybe the method should be generalised a bit more).

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to balearicdynamics

    My interpretation of his question is that he is trying to break the string into four variables.

    So

    1, 0, 1234, 1234,

    would be put into variables

    C, Z, Vpot, Hpot

     

    When using code that defines start and length positions you would extract the final value (Hpot) by looking at a starting point of 12 and a length of 4.

    In the example string supplied above this would be sufficient to get the value 1234.

     

    The issue with position based referencing is that then the third part of the string fell below 1000 e.g.:

    1, 0, 993, 1234,

    the final variable would be missing the first digit and only take the remaining 4 digits "234,"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>