Arduino Forum abut arduino
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 394 subscribers
  • Views 814 views
  • Users 0 members are here
Related

abut arduino

Former Member
Former Member over 9 years ago

a sine wave is applied at a0 using a diode,so that it geets rectified and then after pwm the square obatIned is only with wrt positive cycle ,i need to generate pwm  even during negative cycle and one way is to do it by full bridge rectifier .so is there any way by arduino coding i could get it

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    Yes just measure both positive and negative values during entire cycle.
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    How about offset the sine wave to 50% of VRef (Capacitor coupled will do it, and a divider network), then simply read the whole waveform as a positive value this way 0V = 511 decimal from ADC, -2.5V will…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    How about offset the sine wave to 50% of VRef (Capacitor coupled will do it, and a divider network), then simply read the whole waveform as a positive value

     

    this way 0V = 511 decimal from ADC, -2.5V will be 0 decimal and +2.5V will be 1023

     

    this assumes the input sine wave is appropriatly scaled to a +-2.5V max signal

     

    All the questions Mike asked are still valid though, please provide

     

    You also have not said what resolution you desire to read the values, I am assuming 10 bit based on the built in ADC of the arduino and with my proposed solution, you will have 9 bits in each direction (Simple assume the MSB is a sign bit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    How about offset the sine wave to 50% of VRef (Capacitor coupled will do it, and a divider network), then simply read the whole waveform as a positive value

     

    this way 0V = 511 decimal from ADC, -2.5V will be 0 decimal and +2.5V will be 1023

     

    this assumes the input sine wave is appropriatly scaled to a +-2.5V max signal

     

    All the questions Mike asked are still valid though, please provide

     

    You also have not said what resolution you desire to read the values, I am assuming 10 bit based on the built in ADC of the arduino and with my proposed solution, you will have 9 bits in each direction (Simple assume the MSB is a sign bit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 9 years ago in reply to Robert Peter Oakes

    Peter Oakes & Michael Kellett

    are correct asking for more information as stated.. Also oversample twice the frequency you plan for better accuracy is highly recommended.

    Clem