Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino as isp
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 407 subscribers
  • Views 2192 views
  • Users 0 members are here
  • isp
  • atmelstudio7
Related

Arduino as isp

strb
strb over 9 years ago

Hi, I have to use arduino uno as isp with atmel studio 7, I've upload on arduino the "arduinoasisp" sketch but i can't configure atmel studio to use it as the programmer, I've already found a couple of tutorial but it still doesn't work (probably I'm doing something wrong). Anyone can help me? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 9 years ago +2 suggested
    gihu I have insert the attiny into arduino ide but but when I try to program it it doesn't work. However I have found another solution, it is a little more tricky but it works, it consist on macking the…
  • clem57
    clem57 over 9 years ago +1
    Sure. What steps did you take?
  • gihu
    gihu over 9 years ago in reply to strb +1
    Ciao Steffano, Have you checked this?: Arduino Playground - ArduinoOnOtherAtmelChips So, you can also try to use Arduino IDE if it is easier. Regards
Parents
  • strb
    0 strb over 9 years ago

    gihu I have insert the attiny into arduino ide but but when I try to program it it doesn't work.

     

    However I have found another solution, it is a little more tricky but it works, it consist on macking the program with atmel studio, building it into an hex file and then using the windows command prompt (and avrdude) I send it to arduino that program the attiny.

     

    clem57 gihu thanks a lot for your help and suggestions, I really appreciate them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gihu
    0 gihu over 9 years ago in reply to strb

    That's great you have it working.

    Probably the bwelsby suggestion make it a little bit easier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 9 years ago in reply to strb

    That's great you have it working.

    Probably the bwelsby suggestion make it a little bit easier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • strb
    0 strb over 9 years ago in reply to gihu

    Yes probably it will make the upload easier but even the command line isn't too difficult once learn instructions, I have  programmed only one microcontroller so I'm faster using only the command line compared to set avr studio to make it.

    For future project probably I will do it but not now, thanks to all! image