Arduino Forum Arduino as isp
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
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 393 subscribers
  • Views 1980 views
  • Users 0 members are here
  • isp
  • atmelstudio7
Related

Arduino as isp

strb
strb over 9 years ago

Hi, I have to use arduino uno as isp with atmel studio 7, I've upload on arduino the "arduinoasisp" sketch but i can't configure atmel studio to use it as the programmer, I've already found a couple of tutorial but it still doesn't work (probably I'm doing something wrong). Anyone can help me? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 9 years ago +2 suggested
    gihu I have insert the attiny into arduino ide but but when I try to program it it doesn't work. However I have found another solution, it is a little more tricky but it works, it consist on macking the…
  • clem57
    clem57 over 9 years ago +1
    Sure. What steps did you take?
  • gihu
    gihu over 9 years ago in reply to strb +1
    Ciao Steffano, Have you checked this?: Arduino Playground - ArduinoOnOtherAtmelChips So, you can also try to use Arduino IDE if it is easier. Regards
  • clem57
    0 clem57 over 9 years ago in reply to strb

    avrdude work standalone on command line. I was going to say that next. glad you found it.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bwelsby
    0 bwelsby over 9 years ago in reply to strb

    I haven't used Atmel Studio for a long while but a quick google search and I found this Integrate ArduinoISP and Atmel Studio

    This shows how to add a custom external tool that executes the avrdude command line.

     

    However, if you are happy with the way you have it working then stick with it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 9 years ago in reply to strb

    That's great you have it working.

    Probably the bwelsby suggestion make it a little bit easier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • strb
    0 strb over 9 years ago in reply to gihu

    Yes probably it will make the upload easier but even the command line isn't too difficult once learn instructions, I have  programmed only one microcontroller so I'm faster using only the command line compared to set avr studio to make it.

    For future project probably I will do it but not now, thanks to all! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<