Arduino Forum Please help us with our school project!
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 395 subscribers
  • Views 699 views
  • Users 0 members are here
  • school project
  • stem
  • arduino uno
  • servo
  • arduino
Related

Please help us with our school project!

Former Member
Former Member over 9 years ago

Soo, we have a school project called 'Explore new tech'. For not so tech people...

 

Task:

We'll make a box of Plexiglas that is linked to an android app. In the app, you can create your own to-do lists. When you checked off the chores listed in the app, the box will open, by means of a lock. In the box, you have already put something you would like to have (a reward).

This can be used by e.g. families - the kids have to clean the room before Saturday to get the candy in the box. When the children checked in the boxes in the list the parents have to approve. Then the box will open and they will get their reward.

 

Technology we use:

- An Arduino Uno

- 9v battery

- HC06 bluetooth

- Breadboard

- Servo motor "Futaba S3003"

- Android app

 

Problem:

- The problem is that we want to connect to Bluetooth - the lamp on the bluetooth is flashing but we can't get any communication between the bluetooth and the phone.

- We have obtained the motor to spin, by means of the code bellow. Then we want to have a button for "open" and one for "close" in our android app. So we have got the motor to spin, but we want to control it with open and close buttons. What code shall we use?!

 

We believe we need to put any "if" or "else" code?!

 

I might add that we spent almost a week to checking tutorials now!

 

Is there anyone here who has the skills to help us?
Thanks in advance!

 

// Sweep

// by BARRAGAN <http://barraganstudio.com>

// This example code is in the public domain.

 

 

#include <Servo.h>

 

Servo myservo; // create servo object to control a servo

// a maximum of eight servo objects can be created

 

int pos = 0; // variable to store the servo position

 

void setup()

{

myservo.attach(9); // attaches the servo on pin 9 to the servo object

}

 

 

void loop()

{

for(pos = 0; pos < 180; pos += 1) // goes from 0 degrees to 180 degrees

{ // in steps of 1 degree

myservo.write(pos); // tell servo to go to position in variable 'pos'

delay(15); // waits 15ms for the servo to reach the position

 

 

}

for(pos = 180; pos>=1; pos-=1) // goes from 180 degrees to 0 degrees

{ 

myservo.write(pos); // tell servo to go to position in variable 'pos'

delay(15); // waits 15ms for the servo to reach the position

}

}

  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 9 years ago +1
    Wow, great project idea! I don't have any particular advice myself, but let me promote this post around the Community and see if we can get the experts in to have a look
  • tonyboubady
    tonyboubady over 9 years ago +1
    Generally, projects needs hands-on approach, i can't help it without owning the HC-06 bluetooth module which is pre-programmed with serial port profile. If i own one i would have done the project and send…
Parents
  • gihu
    0 gihu over 9 years ago

    If you have issues with the BT, first check ifyour module HC06 is working.

    Suggest suppling the module, make a short-circuit between Tx and Rx.

    Use any app for making a SPP bluetooth connection and send data over serial, for exemple 'Bluechat'.

    Then connect the app with the module over bluetooth (it is clasical bt, not ble).

    If everything works, any char you send with the app, will be sent and get it back over BT.

    Then it will be time to connect it to the arduino uart, and try a simple program, i.e. open the box when receive 'A', and close when receive 'B'. And check if it works with bluechat, before build your own app.

     

    The described option is with classical bluetooth, with the SPP (serial port profile), you can do it also with BLE, but it works different, and has no spp.

     

    I did an app using bluetooth (spp), I used it with RN42 instead of HC06, but I shoul work equal.

    MODBUS master in my cell phone

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 9 years ago

    If you have issues with the BT, first check ifyour module HC06 is working.

    Suggest suppling the module, make a short-circuit between Tx and Rx.

    Use any app for making a SPP bluetooth connection and send data over serial, for exemple 'Bluechat'.

    Then connect the app with the module over bluetooth (it is clasical bt, not ble).

    If everything works, any char you send with the app, will be sent and get it back over BT.

    Then it will be time to connect it to the arduino uart, and try a simple program, i.e. open the box when receive 'A', and close when receive 'B'. And check if it works with bluechat, before build your own app.

     

    The described option is with classical bluetooth, with the SPP (serial port profile), you can do it also with BLE, but it works different, and has no spp.

     

    I did an app using bluetooth (spp), I used it with RN42 instead of HC06, but I shoul work equal.

    MODBUS master in my cell phone