Arduino Forum Launchpad programming with booster pack attached
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 392 subscribers
  • Views 268 views
  • Users 0 members are here
Related

Launchpad programming with booster pack attached

mr_widget
mr_widget over 9 years ago

I have been working on a special booster pack project (mixed-signal FPGA) for TI MSP430F559 Launchpads.  I have the basic elements of the booster working properly, except each time I wanted to program the Launchpad with Energia I have to remove the booster pack first, or the driver will not be able to download the new code image.  I am wondering if anybody else have experienced the same issue with booster packs and Energia programming.  Is it a matter of DC sag on the USB cable that prevents programming because of the extra load from the booster pack?  If so, does anybody have a workaround?

 

Thanks,

J.R. Stoner

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 9 years ago

    I've not encountered that with "official" TI BoosterPacks.  FPGA's can be power-hungry sometimes, though.

    My first thought would be to use a USB 3.0 port (spec is 750mA vs. 500mA on USB 2.1).

    Clarify, please, which LaunchPad you're using.  The MSP430 series has four digits after MSP430F or MSP430FR.  Some boards are quite particular about the board ID when making a USB connection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago

    This makes sense, because the process of flashing involves an erase cycle before downloading the bytes/hex. The demands on the current become momentarily high and will fail if the juice is running elsewhere. Maybe a cutoff switch to the booster could be used. I would suggest a check if the booster is wasting the current somewhere (leakage or ???).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer