Arduino Forum Launchpad programming with booster pack attached
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 392 subscribers
  • Views 268 views
  • Users 0 members are here
Related

Launchpad programming with booster pack attached

mr_widget
mr_widget over 9 years ago

I have been working on a special booster pack project (mixed-signal FPGA) for TI MSP430F559 Launchpads.  I have the basic elements of the booster working properly, except each time I wanted to program the Launchpad with Energia I have to remove the booster pack first, or the driver will not be able to download the new code image.  I am wondering if anybody else have experienced the same issue with booster packs and Energia programming.  Is it a matter of DC sag on the USB cable that prevents programming because of the extra load from the booster pack?  If so, does anybody have a workaround?

 

Thanks,

J.R. Stoner

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    This makes sense, because the process of flashing involves an erase cycle before downloading the bytes/hex. The demands on the current become momentarily high and will fail if the juice is running elsewhere. Maybe a cutoff switch to the booster could be used. I would suggest a check if the booster is wasting the current somewhere (leakage or ???).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    This makes sense, because the process of flashing involves an erase cycle before downloading the bytes/hex. The demands on the current become momentarily high and will fail if the juice is running elsewhere. Maybe a cutoff switch to the booster could be used. I would suggest a check if the booster is wasting the current somewhere (leakage or ???).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer