Arduino Forum X bee Arduino
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
  • State Not Answered
  • Replies 7 replies
  • Subscribers 403 subscribers
  • Views 724 views
  • Users 0 members are here
  • diy
  • arduino_development_environment
  • uno
  • arduino
  • question
Related

X bee Arduino

Former Member
Former Member over 9 years ago

Hello

 

i have a doubts regarding  the Xbee module.

 

.>What do X-bee modules do? Do they create a wireless serial communication just by configuring them to the arduinos.

eg, i made a simple program for servo control using potentiometer. So if i just attach the 2 X-bee to the two arduinos, will this make it wireless?, will i be able to control the servo wirelessly using potentiometer with the same program.

will i be able to send data wirelessly just by giving a Serial.begin(9600); in the void loop()

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    anshuman kamboj

         The hardware hookup is not to bad using TX/RX pairs. From reading other peoples comments the software configuration was more troublesome. Read carefully and setup mostly according to guide(s). I found  https://learn.adafruit.com/xbee-radios/  to be easy and accurate.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    i saw a project in which the person made a wireless hand controlled robotic hand using 5 servos.(similar to what i am trying to achieve)

    in that he uses 2 X bees and connects them to the 2 arduinos. Then in the program he just writes Serial.begin(9600);in transmitter, and Serial.read in reciever, and that's it . Rest of the program is just for the servo control. How does this work .

     

    I am still not able to figure out how x-bee is working . is it just creating a serial comm between arduinos , just like between pc and single arduino via USB???

    link to that project -How to make a remote controlled Robotic Hand with Arduino - All

    code he has used

    https://codebender.cc/sketch:59559#HandRX_ENG_v2.ino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    To you it is a pipe to send data and receive data. Under the covers the wireless is handled by x-bee firmware. This is like the Internet. We enter a URL and under the covers, translation to first an IP address and later to a physical packet that flows through many like processes until it's arrival at the website. If you want the gory details, there is plenty on Google.

    Clem

    Edit: The serial is a virtual com port. You really do not care so long as the connection works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    so just by connecting X-bee in the way mentioned , will i be able to send data for any device connected to arduino .

    using the way that person did??

    he just connected them and wrote serial.begin(9600);

    can i use that??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    i am sorry if i am asking too immature questions,

    right now i just want it to work , i just want to be able to send data wirelessly just as i do it between my pc and arduino, I am being funded by my college for a project and i just want to know if i should order this so i can develop on it  while i am working on my project. wireless has been a real headache for me.

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    i am sorry if i am asking too immature questions,

    right now i just want it to work , i just want to be able to send data wirelessly just as i do it between my pc and arduino, I am being funded by my college for a project and i just want to know if i should order this so i can develop on it  while i am working on my project. wireless has been a real headache for me.

    Thank you