Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4719 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • ovidiub13
    0 ovidiub13 over 10 years ago

    Thank you for your feedback.

     

    I'm not sure that this schematic works... the led isn't reverse polarized?

    It works.

     

    I've read about how H-bridges work. I understand the general concept. What I'm having issues understanding is how transistors work. Here I'm just using them like switches.

     

    What I've shown previously was, as I've said, half an H-bridge.

     

    Here's the full H-bridge:

     

    image

     

    I've tested this on my breadboard and it works ( I can make a video if necessary).

     

    What I've noticed on the full H-Bridge is that I have 2,77 V on LED1 and 3,40 V on LED2. I don't understand why. SInce the two halves are basically mirrored, I expected them to be the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to ovidiub13

    What I'm having issues understanding is how transistors work

    You can consider a transistor as a switch (in this case they are either ON or OFF)

     

    The control part of the switch is the base to emitter (NPN) or emitter to base (PNP) junction.

    This usually requires 0.6v across it to 'switch' on the Collector to Emitter (NPN) or Emitter to Collector (PNP) junction.

    When in the 'ON' state the C-E/E-C is as low as 0.2v or less in larger devices.

     

    In your half bridge circuit, when you switch S2 on, there is current flow from the +ve through the E-B of Q3 thru R3 and S2 to ground.  ... image

    Q3 is switched ON and current is able to flow through the E-C of Q3, thru LED2 and appears at the Emitter of Q2. ....image

    Current will flow via Q2's E-B, R2 and via Switch2 to ground BUT .... as soon as Q2 turns ON the E-C of Q2 will reduce the voltage to 0.2v at the emitter....image

    Q2 will then be OFF.

    It is likely that the circuit will adjust itself to end up with 0.6v at the Emitter which is not ideal.

     

    BUT the real biggy here is you have effectively dumped 5v across a poor led with no series limiting resistor, which tends to make them very bright for a millisecond.

    You really need to add a 220 ohm resistor in series to stop them being destroyed.

     

     

    The only thing saving your leds and giving the illusion of the circuit working is that Q2 is not turning on and the led current is flowing through the E-B and 330 ohm resistors.

     

     

    Please note

    I have only described one side, but the same could be considered for the other half.

     

    We all start learning somewhere so trying to understand is a great way to learn ...well done.

     

    Mark

     

    BTW

    It's not your fault but generally positve voltages are at the top and ground is at the bottom.

    It tends to come from our right to left and top to bottom reading  ... plus water flows downwards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to ovidiub13

    What I'm having issues understanding is how transistors work

    You can consider a transistor as a switch (in this case they are either ON or OFF)

     

    The control part of the switch is the base to emitter (NPN) or emitter to base (PNP) junction.

    This usually requires 0.6v across it to 'switch' on the Collector to Emitter (NPN) or Emitter to Collector (PNP) junction.

    When in the 'ON' state the C-E/E-C is as low as 0.2v or less in larger devices.

     

    In your half bridge circuit, when you switch S2 on, there is current flow from the +ve through the E-B of Q3 thru R3 and S2 to ground.  ... image

    Q3 is switched ON and current is able to flow through the E-C of Q3, thru LED2 and appears at the Emitter of Q2. ....image

    Current will flow via Q2's E-B, R2 and via Switch2 to ground BUT .... as soon as Q2 turns ON the E-C of Q2 will reduce the voltage to 0.2v at the emitter....image

    Q2 will then be OFF.

    It is likely that the circuit will adjust itself to end up with 0.6v at the Emitter which is not ideal.

     

    BUT the real biggy here is you have effectively dumped 5v across a poor led with no series limiting resistor, which tends to make them very bright for a millisecond.

    You really need to add a 220 ohm resistor in series to stop them being destroyed.

     

     

    The only thing saving your leds and giving the illusion of the circuit working is that Q2 is not turning on and the led current is flowing through the E-B and 330 ohm resistors.

     

     

    Please note

    I have only described one side, but the same could be considered for the other half.

     

    We all start learning somewhere so trying to understand is a great way to learn ...well done.

     

    Mark

     

    BTW

    It's not your fault but generally positve voltages are at the top and ground is at the bottom.

    It tends to come from our right to left and top to bottom reading  ... plus water flows downwards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer