Arduino Forum I need help on my Arduino Nano v3.0
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
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 317 views
  • Users 0 members are here
  • arduino nano
  • error
  • arduino
Related

I need help on my Arduino Nano v3.0

alienozi
alienozi over 9 years ago

Recently I've bought an Arduino Nano and somewhat reason it won't accept my code!

 

Here is the code:

---------------------------------------------------------------------------------------------

int led = 13;

 

//reset

void setup() {               

  pinMode(led, OUTPUT);    

}

 

int i;

int on;

int off;

int pulses;

int cycles = 5;

 

void loop() {

 

  pulses = 8;

  for (on = 1; on <= cycles; on++) {

    for (i = 0; i < pulses; i++) {

      digitalWrite(led, HIGH);  

      delay(on);              

      digitalWrite(led, LOW);   

      delay(cycles - on);              

    }

  

  }

 

  pulses = 8;

  for (off = cycles; off > 1; off--) {

    for (i = 0; i < pulses; i++) {

      digitalWrite(led, HIGH);  

      delay(off);              

      digitalWrite(led, LOW);   

      delay(cycles - off);              

    }

   

  }

 

  digitalWrite(led, LOW);   

  delay(2000);              

}

------------------------------------------------------------------------------------------------------------------------

 

And some Photos of the device. (I couldn't spot a error on the board.)

imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago +1 verified
    What are the error messages in the area below the code ? You can set the IDE to give more information. Under File-Preferences you might want to set the Show verbose output during upload You need to set…
  • mcb1
    mcb1 over 9 years ago in reply to alienozi +1
    I forgot to change that You aren't the first or last to do that one.
  • mcb1
    0 mcb1 over 9 years ago

    What are the error messages in the area below the code ?

    You can set the IDE to give more information.

    image

    Under File-Preferences  you might want to set the Show verbose output during upload

     

    You need to set the board

    image

     

    Plus set the Comm Port.

     

     

    It might also be helpful to tell us what Operating System you're using.

    Otherwise your code compiles okay.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alienozi
    0 alienozi over 9 years ago in reply to mcb1

    Oh thank you! It uploads correctly now. In my recent project I've used UNO, I forgot to change that image mcb1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to alienozi

    I forgot to change that

    You aren't the first or last to do that one.