Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Flora with light sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 6 answers
  • Subscribers 407 subscribers
  • Views 1878 views
  • Users 0 members are here
  • light sensor
  • adafruit_flora
  • neopixels
  • arduino
Related

Arduino Flora with light sensor

Former Member
Former Member over 9 years ago

Hello all.  I am VERY new at Arduino coding, and I am trying to get my Flora and Neopixels to respond using the light sensor.  Something is wrong with my code, and no matter how I try to adjust it, I am still getting errors.  Any help would be appreciated....

And I apologize, but I don't know how to put code tags. 

 

The errors I am getting are the following:

 

(sketch file) light sensor.ino:162:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(255,250,240));

  ^
(sketch file) light sensor.ino:167:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(0,255,0));

  ^
(sketch file) light sensor.ino:172:5: error: use of undeclared identifier 'colorWipe'

  colorWipe(strip.Color(255,0,0));

 

My code so far:

 

#include <Wire.h>

#include <Adafruit_Sensor.h>

#include <Adafruit_TSL2561_U.h>

#include <Adafruit_NeoPixel.h>

 

 

#define PIN 6

Adafruit_NeoPixel strip = Adafruit_NeoPixel(4, PIN, NEO_GRB + NEO_KHZ800);

 

 

 

 

 

 

/* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),

   which provides a common 'type' for sensor data and some helper functions.

  

   To use this driver you will also need to download the Adafruit_Sensor

   library and include it in your libraries folder.

   You should also assign a unique ID to this sensor for use with

   the Adafruit Sensor API so that you can identify this particular

   sensor in any data logs, etc.  To assign a unique ID, simply

   provide an appropriate value in the constructor below (12345

   is used by default in this example).

  

   Connections

   ===========

   Connect SCL to analog 5

   Connect SDA to analog 4

   Connect VDD to 3.3V DC

   Connect GROUND to common ground

   I2C Address

   ===========

   The address will be different depending on whether you leave

   the ADDR pin floating (addr 0x39), or tie it to ground or vcc.

   The default addess is 0x39, which assumes the ADDR pin is floating

   (not connected to anything).  If you set the ADDR pin high

   or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW

   (0x29) respectively.

   

   History

   =======

   2013/JAN/31  - First version (KTOWN)

*/

  

Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);

 

 

/**************************************************************************/

/*

    Displays some basic information on this sensor from the unified

    sensor API sensor_t type (see Adafruit_Sensor for more information)

*/

/**************************************************************************/

void displaySensorDetails(void)

{

  sensor_t sensor;

  tsl.getSensor(&sensor);

  Serial.println("------------------------------------");

  Serial.print  ("Sensor:       "); Serial.println(sensor.name);

  Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);

  Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);

  Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");

  Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");

  Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux"); 

  Serial.println("------------------------------------");

  Serial.println("");

  delay(500);

}

 

 

/**************************************************************************/

/*

    Configures the gain and integration time for the TSL2561

*/

/**************************************************************************/

void configureSensor(void)

{

  /* You can also manually set the gain or enable auto-gain support */

  // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */

  // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */

  tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */

 

  /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */

  tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */

  // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */

  // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */

 

 

  /* Update these values depending on what you've set above! */ 

  Serial.println("------------------------------------");

  Serial.print  ("Gain:         "); Serial.println("Auto");

  Serial.print  ("Timing:       "); Serial.println("13 ms");

  Serial.println("------------------------------------");

}

 

 

 

 

 

 

/**************************************************************************/

/*

    Arduino setup function (automatically called at startup)

*/

/**************************************************************************/

void setup(void)

{

  Serial.begin(9600);

  Serial.println("Light Sensor Test"); Serial.println("");

 

  /* Initialise the sensor */

  if(!tsl.begin())

  {

    /* There was a problem detecting the ADXL345 ... check your connections */

    Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");

    while(1);

  }

 

  /* Display some basic information on this sensor */

  displaySensorDetails();

 

  /* Setup the sensor gain and integration time */

  configureSensor();

 

  /* We're ready to go! */

  Serial.println("");

  

    // This is for Trinket 5V 16MHz, you can remove these three lines if you are not using a Trinket

  #if defined (__AVR_ATtiny85__)

    if (F_CPU == 16000000) clock_prescale_set(clock_div_1);

  #endif

  // End of trinket special code

 

 

 

 

  strip.begin();

  strip.show(); // Initialize all pixels to 'off'

}

 

 

 

 

/**************************************************************************/

/*

    Arduino loop function, called once 'setup' is complete (your own code

    should go here)

*/

/**************************************************************************/

void loop(void)

{

 

 

  /* Get a new sensor event */

  sensors_event_t event;

  tsl.getEvent(&event);

 

  /* Display the results (light is measured in lux) */

  if (event.light)

  {

    Serial.print(event.light); Serial.println(" lux");

  }

  else

  {

    /* If event.light = 0 lux the sensor is probably saturated

       and no reliable data could be generated! */

    Serial.println("Sensor overload");

  }

  delay(250);

 

 

 

 

 

  //>130 is (255, 250, 240)

if (event.light > 130)

{

    colorWipe(strip.Color(255,250,240));

}

// 129-50 is (0,255,0)

else if ((event.light > 50) && (event.light < 129))

{

    colorWipe(strip.Color(0,255,0));

}

// and <50 is (255, 0, 0)

else if (event.light < 50)

{

    colorWipe(strip.Color(255,0,0));

}

 

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 9 years ago +3
    Hey Jennifer, just for future reference, it would be easier if you just copy-pasted the link to your codebender project so that others can look at the code in an easier way, and even compile it to look…
  • Former Member
    Former Member over 9 years ago in reply to mcb1 +3
    yeah sure, i'm not saying it's the only way, or the "right" way, I'm just saying this helps a lot of back and forth questions of "which library version are you using", "do you have that installed", "ok…
  • Former Member
    Former Member over 9 years ago in reply to Former Member +2
    IT'S WORKING!!! I don't know exactly what I did, but thank you all soooo much! mcb1, you are awesome!!! I am completely thrilled, because now I know where I can change things on this code to be able to…
Parents
  • Former Member
    0 Former Member over 9 years ago

    That doesn't remove any of the "no matching function for call to 'colorWipe'" errors, and now I have "note:  candidate function not viable: requires 2 arguments, but 1 was provided".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Okay.  I am back down to one error that says

     

    (sketch file) light sensor 2.ino:142:1: error: expected unqualified-id

    {

     

    (By the way, how do I get my code on my posts to show up in that neat little box?)

     

    My code now looks like this:

     

    #include <Wire.h>

    #include <Adafruit_Sensor.h>

    #include <Adafruit_TSL2561_U.h>

     

     

    /* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),

       which provides a common 'type' for sensor data and some helper functions.

      

       To use this driver you will also need to download the Adafruit_Sensor

       library and include it in your libraries folder.

       You should also assign a unique ID to this sensor for use with

       the Adafruit Sensor API so that you can identify this particular

       sensor in any data logs, etc.  To assign a unique ID, simply

       provide an appropriate value in the constructor below (12345

       is used by default in this example).

      

       Connections

       ===========

       Connect SCL to analog 5

       Connect SDA to analog 4

       Connect VDD to 3.3V DC

       Connect GROUND to common ground

       I2C Address

       ===========

       The address will be different depending on whether you leave

       the ADDR pin floating (addr 0x39), or tie it to ground or vcc.

       The default addess is 0x39, which assumes the ADDR pin is floating

       (not connected to anything).  If you set the ADDR pin high

       or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW

       (0x29) respectively.

       

       History

       =======

       2013/JAN/31  - First version (KTOWN)

    */

      

    Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);

     

     

    /**************************************************************************/

    /*

        Displays some basic information on this sensor from the unified

        sensor API sensor_t type (see Adafruit_Sensor for more information)

    */

    /**************************************************************************/

    void displaySensorDetails(void)

    {

      sensor_t sensor;

      tsl.getSensor(&sensor);

      Serial.println("------------------------------------");

      Serial.print  ("Sensor:       "); Serial.println(sensor.name);

      Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);

      Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);

      Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");

      Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");

      Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux"); 

      Serial.println("------------------------------------");

      Serial.println("");

      delay(500);

    }

     

     

    /**************************************************************************/

    /*

        Configures the gain and integration time for the TSL2561

    */

    /**************************************************************************/

    void configureSensor(void)

    {

      /* You can also manually set the gain or enable auto-gain support */

      // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */

      // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */

      tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */

     

      /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */

      tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */

      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */

      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */

     

     

      /* Update these values depending on what you've set above! */ 

      Serial.println("------------------------------------");

      Serial.print  ("Gain:         "); Serial.println("Auto");

      Serial.print  ("Timing:       "); Serial.println("13 ms");

      Serial.println("------------------------------------");

    }

     

     

    /**************************************************************************/

    /*

        Arduino setup function (automatically called at startup)

    */

    /**************************************************************************/

    void setup(void)

    {

      Serial.begin(9600);

      Serial.println("Light Sensor Test"); Serial.println("");

     

      /* Initialise the sensor */

      if(!tsl.begin())

      {

        /* There was a problem detecting the ADXL345 ... check your connections */

        Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");

        while(1);

      }

     

      /* Display some basic information on this sensor */

      displaySensorDetails();

     

      /* Setup the sensor gain and integration time */

      configureSensor();

     

      /* We're ready to go! */

      Serial.println("");

    }

     

     

    /**************************************************************************/

    /*

        Arduino loop function, called once 'setup' is complete (your own code

        should go here)

    */

    /**************************************************************************/

    void loop()

    { 

      /* Get a new sensor event */

      sensors_event_t event;

      tsl.getEvent(&event);

     

      /* Display the results (light is measured in lux) */

      if (event.light)

      {

        Serial.print(event.light); Serial.println(" lux");

      }

      else

      {

        /* If event.light = 0 lux the sensor is probably saturated

           and no reliable data could be generated! */

        Serial.println("Sensor overload");

      }

      delay(250);

    }

     

    {

     

    //>130 is (255, 250, 240)

    if (event.light > 130)

    {

        colorWipe(strip.Color(255,250,240);

    }

    // 129-50 is (0,255,0)

    else if ((event.light > 50) && (event.light < 129))

    {

        colorWipe(strip.Color(0,255,0);

    }

    // and <50 is (255, 0, 0)

    else if (event.light < 50)

    {

        colorWipe(strip.Color(255,0,0);

     

    }

     

     

    // Fill the dots one after the other with a color

    void colorWipe(uint32_t c, uint8_t wait) {

      for(uint16_t i=0; i<strip.numPixels(); i++) {

        strip.setPixelColor(i, c);

        strip.show();

        delay(wait);

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Okay.  I am back down to one error that says

     

    (sketch file) light sensor 2.ino:142:1: error: expected unqualified-id

    {

     

    (By the way, how do I get my code on my posts to show up in that neat little box?)

     

    My code now looks like this:

     

    #include <Wire.h>

    #include <Adafruit_Sensor.h>

    #include <Adafruit_TSL2561_U.h>

     

     

    /* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),

       which provides a common 'type' for sensor data and some helper functions.

      

       To use this driver you will also need to download the Adafruit_Sensor

       library and include it in your libraries folder.

       You should also assign a unique ID to this sensor for use with

       the Adafruit Sensor API so that you can identify this particular

       sensor in any data logs, etc.  To assign a unique ID, simply

       provide an appropriate value in the constructor below (12345

       is used by default in this example).

      

       Connections

       ===========

       Connect SCL to analog 5

       Connect SDA to analog 4

       Connect VDD to 3.3V DC

       Connect GROUND to common ground

       I2C Address

       ===========

       The address will be different depending on whether you leave

       the ADDR pin floating (addr 0x39), or tie it to ground or vcc.

       The default addess is 0x39, which assumes the ADDR pin is floating

       (not connected to anything).  If you set the ADDR pin high

       or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW

       (0x29) respectively.

       

       History

       =======

       2013/JAN/31  - First version (KTOWN)

    */

      

    Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);

     

     

    /**************************************************************************/

    /*

        Displays some basic information on this sensor from the unified

        sensor API sensor_t type (see Adafruit_Sensor for more information)

    */

    /**************************************************************************/

    void displaySensorDetails(void)

    {

      sensor_t sensor;

      tsl.getSensor(&sensor);

      Serial.println("------------------------------------");

      Serial.print  ("Sensor:       "); Serial.println(sensor.name);

      Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);

      Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);

      Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");

      Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");

      Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux"); 

      Serial.println("------------------------------------");

      Serial.println("");

      delay(500);

    }

     

     

    /**************************************************************************/

    /*

        Configures the gain and integration time for the TSL2561

    */

    /**************************************************************************/

    void configureSensor(void)

    {

      /* You can also manually set the gain or enable auto-gain support */

      // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */

      // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */

      tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */

     

      /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */

      tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */

      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */

      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */

     

     

      /* Update these values depending on what you've set above! */ 

      Serial.println("------------------------------------");

      Serial.print  ("Gain:         "); Serial.println("Auto");

      Serial.print  ("Timing:       "); Serial.println("13 ms");

      Serial.println("------------------------------------");

    }

     

     

    /**************************************************************************/

    /*

        Arduino setup function (automatically called at startup)

    */

    /**************************************************************************/

    void setup(void)

    {

      Serial.begin(9600);

      Serial.println("Light Sensor Test"); Serial.println("");

     

      /* Initialise the sensor */

      if(!tsl.begin())

      {

        /* There was a problem detecting the ADXL345 ... check your connections */

        Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");

        while(1);

      }

     

      /* Display some basic information on this sensor */

      displaySensorDetails();

     

      /* Setup the sensor gain and integration time */

      configureSensor();

     

      /* We're ready to go! */

      Serial.println("");

    }

     

     

    /**************************************************************************/

    /*

        Arduino loop function, called once 'setup' is complete (your own code

        should go here)

    */

    /**************************************************************************/

    void loop()

    { 

      /* Get a new sensor event */

      sensors_event_t event;

      tsl.getEvent(&event);

     

      /* Display the results (light is measured in lux) */

      if (event.light)

      {

        Serial.print(event.light); Serial.println(" lux");

      }

      else

      {

        /* If event.light = 0 lux the sensor is probably saturated

           and no reliable data could be generated! */

        Serial.println("Sensor overload");

      }

      delay(250);

    }

     

    {

     

    //>130 is (255, 250, 240)

    if (event.light > 130)

    {

        colorWipe(strip.Color(255,250,240);

    }

    // 129-50 is (0,255,0)

    else if ((event.light > 50) && (event.light < 129))

    {

        colorWipe(strip.Color(0,255,0);

    }

    // and <50 is (255, 0, 0)

    else if (event.light < 50)

    {

        colorWipe(strip.Color(255,0,0);

     

    }

     

     

    // Fill the dots one after the other with a color

    void colorWipe(uint32_t c, uint8_t wait) {

      for(uint16_t i=0; i<strip.numPixels(); i++) {

        strip.setPixelColor(i, c);

        strip.show();

        delay(wait);

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    it looks like my reply is out of order now  ... see above inc how to use the syntax highlighter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to mcb1

    Okay, I added the wait value.  Now I have these errors:

     

    (sketch file) light sensor 2.ino:140:1: error: expected unqualified-id

    if (event.light > 130)

    ^
    (sketch file) light sensor 2.ino:145:1: error: expected unqualified-id

    else if ((event.light > 50) && (event.light < 129))

    ^
    (sketch file) light sensor 2.ino:150:1: error: expected unqualified-id

    else if (event.light < 50)

    ^
    (sketch file) light sensor 2.ino:159:23: error: use of undeclared identifier 'strip'

      for(uint16_t i=0; i<strip.numPixels(); i++) {

      ^
    (sketch file) light sensor 2.ino:160:5: error: use of undeclared identifier 'strip'

      strip.setPixelColor(i, c);

      ^
    (sketch file) light sensor 2.ino:161:5: error: use of undeclared identifier 'strip'

      strip.show();

     

    #include <Wire.h>
    #include <Adafruit_Sensor.h>
    #include <Adafruit_TSL2561_U.h>
    
    
    /* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),
       which provides a common 'type' for sensor data and some helper functions.
       
       To use this driver you will also need to download the Adafruit_Sensor
       library and include it in your libraries folder.
       You should also assign a unique ID to this sensor for use with
       the Adafruit Sensor API so that you can identify this particular
       sensor in any data logs, etc.  To assign a unique ID, simply
       provide an appropriate value in the constructor below (12345
       is used by default in this example).
       
       Connections
       ===========
       Connect SCL to analog 5
       Connect SDA to analog 4
       Connect VDD to 3.3V DC
       Connect GROUND to common ground
       I2C Address
       ===========
       The address will be different depending on whether you leave
       the ADDR pin floating (addr 0x39), or tie it to ground or vcc.
       The default addess is 0x39, which assumes the ADDR pin is floating
       (not connected to anything).  If you set the ADDR pin high
       or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW
       (0x29) respectively.
        
       History
       =======
       2013/JAN/31  - First version (KTOWN)
    */
       
    Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);
    
    
    /**************************************************************************/
    /*
        Displays some basic information on this sensor from the unified
        sensor API sensor_t type (see Adafruit_Sensor for more information)
    */
    /**************************************************************************/
    void displaySensorDetails(void)
    {
      sensor_t sensor;
      tsl.getSensor(&sensor);
      Serial.println("------------------------------------");
      Serial.print  ("Sensor:       "); Serial.println(sensor.name);
      Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);
      Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);
      Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");
      Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");
      Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux");  
      Serial.println("------------------------------------");
      Serial.println("");
      delay(500);
    }
    
    
    /**************************************************************************/
    /*
        Configures the gain and integration time for the TSL2561
    */
    /**************************************************************************/
    void configureSensor(void)
    {
      /* You can also manually set the gain or enable auto-gain support */
      // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */
      // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */
      tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */
      
      /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */
      tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */
      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */
      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */
    
    
      /* Update these values depending on what you've set above! */  
      Serial.println("------------------------------------");
      Serial.print  ("Gain:         "); Serial.println("Auto");
      Serial.print  ("Timing:       "); Serial.println("13 ms");
      Serial.println("------------------------------------");
    }
    
    
    /**************************************************************************/
    /*
        Arduino setup function (automatically called at startup)
    */
    /**************************************************************************/
    void setup(void) 
    {
      Serial.begin(9600);
      Serial.println("Light Sensor Test"); Serial.println("");
      
      /* Initialise the sensor */
      if(!tsl.begin())
      {
        /* There was a problem detecting the ADXL345 ... check your connections */
        Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");
        while(1);
      }
      
      /* Display some basic information on this sensor */
      displaySensorDetails();
      
      /* Setup the sensor gain and integration time */
      configureSensor();
      
      /* We're ready to go! */
      Serial.println("");
    }
    
    
    /**************************************************************************/
    /*
        Arduino loop function, called once 'setup' is complete (your own code
        should go here)
    */
    /**************************************************************************/
    void loop() 
    {  
      /* Get a new sensor event */ 
      sensors_event_t event;
      tsl.getEvent(&event);
    
      /* Display the results (light is measured in lux) */
      if (event.light)
      {
        Serial.print(event.light); Serial.println(" lux");
      }
      else
      {
        /* If event.light = 0 lux the sensor is probably saturated
           and no reliable data could be generated! */
        Serial.println("Sensor overload");
      }
      delay(250);
    
    
    }
    
    
    //>130 is (255, 250, 240)
    if (event.light > 130)
    {
        colorWipe(strip.Color(255,250,240), 50);
    }
    // 129-50 is (0,255,0)
    else if ((event.light > 50) && (event.light < 129))
    {
        colorWipe(strip.Color(0,255,0), 50);
    }
    // and <50 is (255, 0, 0) 
    else if (event.light < 50)
    {

     

     

    THANK YOU for teaching me how to put it in a box!!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    IT'S WORKING!!! I don't know exactly what I did, but thank you all soooo much!   mcb1, you are awesome!!!  I am completely thrilled, because now I know where I can change things on this code to be able to use it for more than one variation.  THANK YOU, THANK YOU, THANK YOU!!!!

     

    Final code:

     

    #include <Wire.h>
    #include <Adafruit_Sensor.h>
    #include <Adafruit_TSL2561_U.h>
    #include <Adafruit_NeoPixel.h>
    
    
    #define PIN 6
    Adafruit_NeoPixel strip = Adafruit_NeoPixel(4, PIN, NEO_GRB + NEO_KHZ800);
    
    
    
    
    
    
    /* This driver uses the Adafruit unified sensor library (Adafruit_Sensor),
       which provides a common 'type' for sensor data and some helper functions.
      
       To use this driver you will also need to download the Adafruit_Sensor
       library and include it in your libraries folder.
       You should also assign a unique ID to this sensor for use with
       the Adafruit Sensor API so that you can identify this particular
       sensor in any data logs, etc.  To assign a unique ID, simply
       provide an appropriate value in the constructor below (12345
       is used by default in this example).
      
       Connections
       ===========
       Connect SCL to analog 5
       Connect SDA to analog 4
       Connect VDD to 3.3V DC
       Connect GROUND to common ground
       I2C Address
       ===========
       The address will be different depending on whether you leave
       the ADDR pin floating (addr 0x39), or tie it to ground or vcc.
       The default addess is 0x39, which assumes the ADDR pin is floating
       (not connected to anything).  If you set the ADDR pin high
       or low, use TSL2561_ADDR_HIGH (0x49) or TSL2561_ADDR_LOW
       (0x29) respectively.
       
       History
       =======
       2013/JAN/31  - First version (KTOWN)
    */
      
    Adafruit_TSL2561_Unified tsl = Adafruit_TSL2561_Unified(TSL2561_ADDR_FLOAT, 12345);
    
    
    /**************************************************************************/
    /*
        Displays some basic information on this sensor from the unified
        sensor API sensor_t type (see Adafruit_Sensor for more information)
    */
    /**************************************************************************/
    void displaySensorDetails(void)
    {
      sensor_t sensor;
      tsl.getSensor(&sensor);
      Serial.println("------------------------------------");
      Serial.print  ("Sensor:       "); Serial.println(sensor.name);
      Serial.print  ("Driver Ver:   "); Serial.println(sensor.version);
      Serial.print  ("Unique ID:    "); Serial.println(sensor.sensor_id);
      Serial.print  ("Max Value:    "); Serial.print(sensor.max_value); Serial.println(" lux");
      Serial.print  ("Min Value:    "); Serial.print(sensor.min_value); Serial.println(" lux");
      Serial.print  ("Resolution:   "); Serial.print(sensor.resolution); Serial.println(" lux"); 
      Serial.println("------------------------------------");
      Serial.println("");
      delay(500);
    }
    
    
    /**************************************************************************/
    /*
        Configures the gain and integration time for the TSL2561
    */
    /**************************************************************************/
    void configureSensor(void)
    {
      /* You can also manually set the gain or enable auto-gain support */
      // tsl.setGain(TSL2561_GAIN_1X);      /* No gain ... use in bright light to avoid sensor saturation */
      // tsl.setGain(TSL2561_GAIN_16X);     /* 16x gain ... use in low light to boost sensitivity */
      tsl.enableAutoRange(true);            /* Auto-gain ... switches automatically between 1x and 16x */
    
      /* Changing the integration time gives you better sensor resolution (402ms = 16-bit data) */
      tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_13MS);      /* fast but low resolution */
      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_101MS);  /* medium resolution and speed   */
      // tsl.setIntegrationTime(TSL2561_INTEGRATIONTIME_402MS);  /* 16-bit data but slowest conversions */
    
    
      /* Update these values depending on what you've set above! */ 
      Serial.println("------------------------------------");
      Serial.print  ("Gain:         "); Serial.println("Auto");
      Serial.print  ("Timing:       "); Serial.println("13 ms");
      Serial.println("------------------------------------");
    }
    
    
    
    
    
    
    /**************************************************************************/
    /*
        Arduino setup function (automatically called at startup)
    */
    /**************************************************************************/
    void setup(void)
    {
      Serial.begin(9600);
      Serial.println("Light Sensor Test"); Serial.println("");
    
      /* Initialise the sensor */
      if(!tsl.begin())
      {
        /* There was a problem detecting the ADXL345 ... check your connections */
        Serial.print("Ooops, no TSL2561 detected ... Check your wiring or I2C ADDR!");
        while(1);
      }
    
      /* Display some basic information on this sensor */
      displaySensorDetails();
    
      /* Setup the sensor gain and integration time */
      configureSensor();
    
      /* We're ready to go! */
      Serial.println("");
      
        // This is for Trinket 5V 16MHz, you can remove these three lines if you are not using a Trinket
      #if defined (__AVR_ATtiny85__)
        if (F_CPU == 16000000) clock_prescale_set(clock_div_1);
      #endif
      // End of trinket special code
    
    
    
    
      strip.begin();
      strip.show(); // Initialize all pixels to 'off'
    }
    
    
    
    
    /**************************************************************************/
    /*
        Arduino loop function, called once 'setup' is complete (your own code
        should go here)
    */
    /**************************************************************************/
    void loop(void)
    {
    
    
      /* Get a new sensor event */
      sensors_event_t event;
      tsl.getEvent(&event);
    
      /* Display the results (light is measured in lux) */
      if (event.light)
      {
        Serial.print(event.light); Serial.println(" lux");
      }
      else
      {
        /* If event.light = 0 lux the sensor is probably saturated
           and no reliable data could be generated! */
        Serial.println("Sensor overload");
      }
      delay(250);
    
    
    
    
    
      //>130 is (255, 250, 240)
    if (event.light > 130)
    {
        colorWipe(strip.Color(255,250,240), 50);
    }
    // 129-50 is (0,255,0)
    else if ((event.light > 50) && (event.light < 129))
    {
        colorWipe(strip.Color(0,255,0), 50);
    }
    // and <50 is (255, 0, 0)
    else if (event.light < 50)
    {
        colorWipe(strip.Color(255,0,0), 50);
    }
    
    
    }
    
    
    // Fill the dots one after the other with a color  
    void colorWipe(uint32_t c, uint8_t wait) {  
      for(uint16_t i=0; i<strip.numPixels(); i++) {  
          strip.setPixelColor(i, c);  
          strip.show();  
          delay(wait);  
      }  
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    Your errors are because you have a bunch of commands outside the Void loop()

    Your start { is at line 125 while the close } is at 144

     

    But then you have other code at lines 147-159 which should have been inside the loop.

     

    You fixed that with the second post (you moved it to line 193)   image

     

     

    A handy trick of the new IDE's is that if you click on the bracket (start or finish), it highlights the matching one.

    Whether it does this in codebender or not I'm not sure.

     

    Another helpful way is indenting.

    While you don't need to, it makes the code much easier to follow and debug the odd missing bits.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to Former Member

    BTW

    Others may not appreciate you marking your own answer as correct after getting help.

     

    Glad you've been able to learn some new tricks.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer