What is the easiest way to talk to multiple slave devices using and Arduino platform (or TI Energia platform). the issue I am thinking about is having to keep passing the new CS pin the SPI begin function. Any help is much appreciated.
Thanks
Kas
What is the easiest way to talk to multiple slave devices using and Arduino platform (or TI Energia platform). the issue I am thinking about is having to keep passing the new CS pin the SPI begin function. Any help is much appreciated.
Thanks
Kas
Hi Kas!
I don't think I've done it with these platforms, but on others I've usually done it "out-of-band" so to speak, i.e. control the various CS pins using digitalWrite or whatever (not using the SPI API), and then invoke the SPI API commands as usual to perform the data transfer.
In other words, SPI API and my digitalWrite operate like ships in the night. Maybe not the best way, but it seemed straightforward.
The API's in Arduino/Energia may be richer, but if they are not, then maybe a digitalWrite method is sufficient.
Your question exposes the limitations of using "out of the box" library functions to control hardware - one is always at the mercy of the choices and simplifications made when the function was written.
All is not lost - the Arduino stuff is open source so you can modify the SPI driver for the slave so that the MISO pin is tri-stated when the port is at rest. Then you can devise a protocol which allows the master to address a slave to talk - so that the slave then activates its MISO pin. This way you can wire many slaves in parallel, subject only to the limitations of hardware.
The downside of this approach is that every slave must be able to see the "address to talk" messages from the master - which will add to the processing load on them - but in many cases this isn't a problem.
If the slave devices are just dumb chips this system won't be possible - my solution then would be to use Shabaz's method, or a modern processor which will have multiple SPI ports, or be fast enough to bit bang as many as you might want.
MK
Thank you for the responce, I have not used Emergia or Arduino that much, I prefer barebones... That being said I would really need to spend some time to learn how to edit the library to include a CS pin to set high or low in teh function call.
It is this reason I have kept away from Energia and Arduino I find it very confining and restricting in what and how I can do things.
Thank you for the suggestions and the help
Kas
Kas, you can take this for what it's worth. You see you want a broadcast mode, but you already limited yourself to SPI.
This is like; Cart before Horse. You should have asked yourself; What do I need?
And then no matter what Communications Hardware or Firmware you have, you have to implement a protocol.
SPI, I2C have rather short distances it can go, even though I2C has reserved address. they are both on the weak side.
for CHEAP a few bucks each on ebay i picked up some I2C to CAN bus transceivers. This has broadcast and does about 40 feet on twisted pair.
Dehumidifier messages:
1 The Temp is xxx
2 The Humidify is xxx
3 The Tank is Full
4 The Tank is not in place
System messages to the Dehumidifier
5 Turn ON
6 Turn OFF
This is the protocol: bit 0 to bit n Numbers are in HEX
FF fist two bytes - Start Byte
01 second two bytes Device # this is the Dehumidifier.
xx third two bytes Message Code
xx forth two bytes the Message or Payload
00 fifth two bytes Stop Byte
Cris
PS and to anybody that takes a known standard and wants to hack it by adding another "control wire".... I had a real problem I used to make the board myself
NOW I JUST BUY THEM...LOL