Arduino Forum Multiple SPI Slaves
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
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 401 subscribers
  • Views 1013 views
  • Users 0 members are here
Related

Multiple SPI Slaves

kas.lewis
kas.lewis over 9 years ago

What is the easiest way to talk to multiple slave devices using and Arduino platform (or TI Energia platform). the issue I am thinking about is having to keep passing the new CS pin the SPI begin function. Any help is much appreciated.

 

Thanks

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +2
    Your question exposes the limitations of using "out of the box" library functions to control hardware - one is always at the mercy of the choices and simplifications made when the function was written…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Kas!

     

    I don't think I've done it with these platforms, but on others I've usually done it "out-of-band" so to speak, i.e. control the various CS pins using digitalWrite or whatever (not using the SPI API), and then invoke the SPI API commands as usual to perform the data transfer.

     

    In other words, SPI API and my digitalWrite operate like ships in the night. Maybe not the best way, but it seemed straightforward.

    The API's in Arduino/Energia may be richer, but if they are not, then maybe a digitalWrite method is sufficient.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Kas!

     

    I don't think I've done it with these platforms, but on others I've usually done it "out-of-band" so to speak, i.e. control the various CS pins using digitalWrite or whatever (not using the SPI API), and then invoke the SPI API commands as usual to perform the data transfer.

     

    In other words, SPI API and my digitalWrite operate like ships in the night. Maybe not the best way, but it seemed straightforward.

    The API's in Arduino/Energia may be richer, but if they are not, then maybe a digitalWrite method is sufficient.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer