Arduino
  • Products
  • More
Arduino
Arduino Forum Detect whether a pin is connected to GND
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 8 answers
  • Subscribers 416 subscribers
  • Views 3880 views
  • Users 0 members are here
  • arduino uno
  • iot
Related

Detect whether a pin is connected to GND

tim687
tim687 over 9 years ago

Hi everyone!

 

Recently I've started working on my own IoT project. An Airco that has no connectivity to the world (except for a remote, that I never use), to connect it to the internet.

 

Note: The Arduino Uno is connected with an NodeMCU ESP-12F via serial. The Arduino Uno communicates with the AC circuitry.

 

However, I'm facing a serious problem that stops me from continuing with the project.

 

The AC has got three modes, Cool, Dry and Fan. Microprocessor controls the specialised equipment inside the AC (such as the refrig., the pump etc) so there is no line going to the other control board that is high when one of the three modes is active.

The MIP (microprocessor) controls three leds to let the user know which mode is active. (here comes the, for me, very difficult part)

The GND connections of the LED's are connected to the MIP (pulls, I guess) and they are being connected to GND when a mode is active.

The challenge for me, with my Arduino Uno, is to check which GND connection of the three LED's is connected to the GND line of the external circuitry.

 

I've made a beginning, for each line I've used this setup:

 

image

My selfmade and NOT complete schematic of the AC circuit

image

 

The values I get are usable, but they require taking loads of samples, and taking the average of all the samples, to check which line has got the lowest value (and thus is connected to GND). However, the values are fluctuating very much, and are not very accurate.

As required, the GND of the Arduino is connected to the GND of the AC circuitry.

 

If you want to see a few pictures of the AC circuitry, check out my Google Drive here.

 

The project is a hobby project, next to my school projects, so there is no deadline or something image

 

Thank you in advance for your help,

 

Tim

 

Message was edited by: Tim Koers Added the AC circuitry schematic

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 9 years ago in reply to tim687 +2 suggested
    If you're going to do all that, I think it would be worth your while sitting down with large sheet of paper and drawing out the circuit. It should be easy to do - you can see all the tracks, and the conventional…
  • jc2048
    jc2048 over 9 years ago +1 suggested
    Are you sure the drive is direct. [It's difficult to make out from your photographs because of the large blob of silicone over the capacitor that they've added.] The processor (assuming it is a processor…
Parents
  • tim687
    0 tim687 over 9 years ago

    I've added a few photo's of the back of the PCB. I had removed the glue blob a while ago but didn't add new photos of it.

    I've also thought about matrixing, what I do know is that the 7 segment (2 dig.) display is being driven by the shift register next to it. That might be the case for the LEDs to, that the shift register is matrixing the LEDs + connection.

    I was already planning to (somehow) read the serial input of the sr because I want to know what is on the screen.

     

    Thanks,

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 9 years ago in reply to tim687

    If you're going to do all that, I think it would be worth your while sitting down with large sheet of paper and drawing out the circuit. It should be easy to do - you can see all the tracks, and the conventional components are simple to recognise. It will make it much more straightforward to plan your modifications. You'll also get more answers here because many of us can read schematics quickly but don't have the time (or inclination) to trace out a circuit from photographs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 9 years ago in reply to tim687

    If you're going to do all that, I think it would be worth your while sitting down with large sheet of paper and drawing out the circuit. It should be easy to do - you can see all the tracks, and the conventional components are simple to recognise. It will make it much more straightforward to plan your modifications. You'll also get more answers here because many of us can read schematics quickly but don't have the time (or inclination) to trace out a circuit from photographs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer