Arduino Forum ESP 01 overheating
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
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 3395 views
  • Users 0 members are here
  • internet of thins
  • overheating
  • esp 01
  • esp8266
Related

ESP 01 overheating

alphaallan
alphaallan over 9 years ago

Hello everyone, i am running a small project using an ESP 01, every thing has working fine when out of the nowhere the ESP started to overheat. At first i thought that i had made something wrong with the power supply and/or program (i had fried a PIC 16F877A in pass just because of a typo), but a checked every thing and i didn't mess up this time, in fact even the blink example for the ESP makes it goes really hot now.

The circuit is an remote control for two relays, managed by an ESP 01 powered by an dedicated 3V3 power supply (for the ESP only) with the GPIO0 and GPIO2 hooked to a pair of optocouplers with 130R resistors, the program uses the aREST and aREST UI API.

if anyone can tell me what maybe happen and if it can be fixed, i will be glad. 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +2 suggested
    Hi Allan, Detail is needed.. high quality photos of your set-up, and ideally a circuit diagram if possible, and let people know what tools you have access to, in order to troubleshoot. The editor tools…
Parents
  • DAB
    0 DAB over 9 years ago

    You need to look at your IO and see if you are overdrawing current.

     

    I suspect that you have too small a resistor somewhere or an unexpected short that is causing the excess current draw, and hence the overheating.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alphaallan
    0 alphaallan over 9 years ago in reply to DAB

    Done that, and the chip overheats even with no load. I'm suspecting of an internal short circuit (seams to be the only plausible explanation), but still no glue how it happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alphaallan
    0 alphaallan over 9 years ago in reply to DAB

    Done that, and the chip overheats even with no load. I'm suspecting of an internal short circuit (seams to be the only plausible explanation), but still no glue how it happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 9 years ago in reply to alphaallan

    Hi allan,

    I have seen this happen in other chips. Based on what you have said and tested you likely have a polarity or other protection diode in the chips architecture that has failed. If you have a way to look at the current the bad one is using compared to the current a good one is using you will see where the heat is coming from. While the chip may continue to work OK for a while the heat will eventually be a death blow to it. It is best to replace it as you do not want it to fail when it is doing something important.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer