Arduino Forum What do mean by arrays?
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
  • State Not Answered
  • Replies 9 replies
  • Subscribers 403 subscribers
  • Views 960 views
  • Users 0 members are here
  • processing
  • arudino
Related

What do mean by arrays?

topaz
topaz over 9 years ago

Over 5 days this question remained in my mind "What do mean by arrays"?

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 9 years ago +1
    A simple way to think about Array's is to look at an old record Juke box. You have a series of records or CD's lined up along the selection cabinet. When you enter the code for the CD you want, the mechanism…
  • D_Hersey
    D_Hersey over 9 years ago in reply to DAB +1
    I certainly wasn't trying to correct you, DAB. Just trying to throw in a fun fact. Any linear ordering of data for which we can perform comparison operations on the indices, so long as they are unique…
  • DAB
    DAB over 9 years ago in reply to D_Hersey +1
    No problem, I was just making sure that we answered the question of an obvious newbie with simple explanations. There is plenty of time to bring them over to the dark side later. DAB
Parents
  • jgerred
    0 jgerred over 9 years ago

    Basically an array is a variable that holds multiple values.  For instance a single variable called "a" can hold a single value as in "a=1".  Turning that variable into an array makes it sort of like a list of values that are accessible via that same variable name but with an index added (most arrays are zero indexed), for example a="9 5 6 3 2" gives us a[0]=9, a[1]=5, a[2]=6, a[3]=3, a[4]=2.  You can also assign a value to an array index directly, for example a[4]=5 would change the value in the slot a[4] from a 2 to a 5.  How you initialize and populate an array variable varies depending on which language you are using, but they all behave basically the same way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jgerred
    0 jgerred over 9 years ago

    Basically an array is a variable that holds multiple values.  For instance a single variable called "a" can hold a single value as in "a=1".  Turning that variable into an array makes it sort of like a list of values that are accessible via that same variable name but with an index added (most arrays are zero indexed), for example a="9 5 6 3 2" gives us a[0]=9, a[1]=5, a[2]=6, a[3]=3, a[4]=2.  You can also assign a value to an array index directly, for example a[4]=5 would change the value in the slot a[4] from a 2 to a 5.  How you initialize and populate an array variable varies depending on which language you are using, but they all behave basically the same way.