Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Program an Arduino with another Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 7 answers
  • Subscribers 421 subscribers
  • Views 2763 views
  • Users 0 members are here
  • arduino
  • programmer
Related

Program an Arduino with another Arduino

rishi2628
rishi2628 over 9 years ago

image

 

Is there any way I can program an Arduino using another Arduino,without the need of any computer. I want to store the programming code in the EEPROM of the "Programmer Arduino" and using any interface like SPI, I2C or Serial, burn this code to the Second arduino. Is it possible and how can it be implemented ?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 9 years ago in reply to clem57 +2 suggested
    clem57 That link is for programming the bootloader into a blank 328 chip. If I read the OP right, he wants to use an Arduino to replace the program contents. I'm sure there is a method of poking data onto…
  • rishi2628
    rishi2628 over 9 years ago +1 suggested
    Actually I was looking for a solution something like this :- https://www.youtube.com/watch?v=M-sFQNIXde8
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    How to program using SPI like interface is all in the UserGuide for the chip

    http://www.atmel.com/images/Atmel-8271-8-bit-AVR-Microcontroller-ATmega48A-48PA-88A-88PA-168A-168PA-328-328P_datasheet_C…

    1. Write the sketch or modify existing one such that when powered on a d perhaps a button is pressed, it will try to start programming an attached ATMEGA328 (Using its pins 10, 11,12,13)

    now every time the programmer is powered on, it will wait for a button press and then execute the programed sequence to transfer the desired program to the target.

     

    You will have to program the target code as a binary file separately, convert it into a byte array in your code and on command, transfer this to the flash memory of the target ATMEGA.

     

    Obviously you will never be able to have a program as big as its flash as the source is stored in FLASH along with the code to program another. You could use an ATMEGA2560 to overcome this limitation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    How to program using SPI like interface is all in the UserGuide for the chip

    http://www.atmel.com/images/Atmel-8271-8-bit-AVR-Microcontroller-ATmega48A-48PA-88A-88PA-168A-168PA-328-328P_datasheet_C…

    1. Write the sketch or modify existing one such that when powered on a d perhaps a button is pressed, it will try to start programming an attached ATMEGA328 (Using its pins 10, 11,12,13)

    now every time the programmer is powered on, it will wait for a button press and then execute the programed sequence to transfer the desired program to the target.

     

    You will have to program the target code as a binary file separately, convert it into a byte array in your code and on command, transfer this to the flash memory of the target ATMEGA.

     

    Obviously you will never be able to have a program as big as its flash as the source is stored in FLASH along with the code to program another. You could use an ATMEGA2560 to overcome this limitation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer