Arduino Forum Replacing a device's button with an Arduino
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
  • State Verified Answer
  • Replies 30 replies
  • Answers 11 answers
  • Subscribers 393 subscribers
  • Views 5021 views
  • Users 0 members are here
  • arduino uno
  • arduino_tutorials
  • advice
  • costume
Related

Replacing a device's button with an Arduino

talongrayson
talongrayson over 8 years ago

Hi,

 

Let me start by saying that I'm fairly new to electronics, and I may get some terminology wrong in this post. I'll do my best to ensure it makes sense, though, and please feel free to correct me where necessary as I am very keen to learn.

 

As the title (vaguely) suggests, I am working on a project in which I need to - for want of a better description - replace a device's 'push to make' switch with an Arduino Uno.

 

The project is actually the glove of a costume I am building. It is going to release 'smoke' when the wearer's hand is in specified positions. The setup isn't hugely complicated, and I believe I have everything straight in my head except for one thing. I'll start by explaining the setup...


In the glove I have an accelerometer, and with my Arduino sketch I can define gestures and recognise those gestures.

 

I've built a basic shield for the Arduino with a transistor so that I can control a blower fan. The Arduino and fan are powered by a 9v battery which connects to this shield. I've essentially enclosed the blower fan so that its inlet is connected to a 'vape' (you know, one of those e-cigarette type things).


So far I have got everything working, but the vape is not connected to the Arduino in any way. In fact, it hasn't even arrived yet, so while awaiting its delivery I've been considering how I might connect it all up.

The intention is to have the fan and some LEDs turn on and the vape button pressed when a specific gesture is made. The vape will heat up, the fan will suck vapor through the tubes, and the vapor will emerge from the glove. When the gesture is no longer being made, the fan turns off and the vape button is released.

 

I've gone through a couple of options in my head, including things like having the Arduino control a servo which mechanically presses the button on the vape, but what I'd really like is it pretty much desolder the vape's switch, remove it from the vape, and solder wire at its connections which then connect to the Arduino... or thereabouts, if you see what I mean.

 

So I'm here to get some advice on what would be the best way to approach this. Is it possible? Trivial? Will I need to use a transistor, a DAC, a relay, or some other method?

 

Any help would be greatly appreciated and I am more than happy to elaborate further if needs be.

  • Sign in to reply
  • Cancel

Top Replies

  • talongrayson
    talongrayson over 8 years ago +3
    The reed relay arrived today. To cut a long story short, it works like a charm. Next step is to migrate that part of the circuit to the shield. In due course I will upload photos/video to show it in action;…
  • jlangbridge
    jlangbridge over 8 years ago in reply to talongrayson +2 verified
    Aha... So there is a bit of logic there, this isn't a simple on/off switch (I'm not a vaper either, so I had no idea). Well, maybe the "easiest" solution would be to use a relay. There are several types…
  • jlangbridge
    jlangbridge over 8 years ago in reply to talongrayson +2
    Possibly, but I still need a bit of information first; the amount of power required to activate the switch. The relay itself is powered by a coil, and that coil requires power, but a lot of relays require…
Parents
  • talongrayson
    0 talongrayson over 8 years ago

    Hello again!

     

    Apologies to bump a thread unnecessarily - I just wanted to assure anyone who's still interested that I haven't forgotten about my intention to share this project. It's been a very busy couple of months; not sure if I mentioned it previously but my wife and I are renewing our wedding vows at the end of this month, which is what the costume is for. So aside from the costume being ambitious, there is basically a whole wedding which has been organised in parallel.

     

    The costume is almost complete, and I think the glove is pretty much done, with the exception of fine tuning some of the gestures in code, and such. I plan to document the glove assembly as fully as possible over the next week or two (better to get the photos before the drinking begins, right?) and share everything during May.

     

    Ahead of that, could someone inform me of this forum's preferred method of sharing, please? Should I just attached photos, the sketch, and so forth directly to a post, for example?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlangbridge
    0 jlangbridge over 8 years ago in reply to talongrayson

    Glad to see you back! I would say post it as a blog post, along with photos, code, and anything you think could be interesting to explain the project. Apparently, there is a new project where you can win stuff for blog posts on the e14 website... So try, and see what happens! Looking forward to reading about it, and good luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jlangbridge
    0 jlangbridge over 8 years ago in reply to talongrayson

    Glad to see you back! I would say post it as a blog post, along with photos, code, and anything you think could be interesting to explain the project. Apparently, there is a new project where you can win stuff for blog posts on the e14 website... So try, and see what happens! Looking forward to reading about it, and good luck!

    • Cancel
    • Vote Up +2 Vote Down