Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 16x2 LCD i2c sketch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 850 views
  • Users 0 members are here
Related

16x2 LCD i2c sketch

nealbopper
nealbopper over 9 years ago

Hello all,

I have started on my automatic Chicken coop door project. Woo Hoo!

I had no issues with loading the Arduino files, I had no issues setting up my RTC and I set the time.

This is a big step for this newbie. LOL I got a 16x2 LCD with a I2c piggyback. I am having a real arduous

time trying to find the port code so I can upload my info.

Question 1:

Is there a way to clear all the uploads you have made to the Uno? I think I made allot of unnecessary uploads.

2.) I have the PCF8574T chip on my UXCELL 5v display. I have power and the first row is just solid white squares.

     I have adjusted the contrast but I see no letters. I have uploaded the i2C scanner but all it displays is Searching.......

     on the read out.

3.) Does anybody have a clue what I need to do because I am lost. With a 5v source I wouldn't think I need any resistors.

     Any help would be greatly appreciated.

 

FYI, If you want to run your Uno on 12v solar power, just connect it to the, "Vin" port. That converts your 12 v to 5v.

FYI. A L298N motor controller CAN run 2 separate drill motors.

Thank for all your help so far.

  • Sign in to reply
  • Cancel
  • the-dubster
    0 the-dubster over 9 years ago

    Unless I'm reading this wrong, to clear previous sketches, upload the following null sketch.

     

     

    void setup() {}

    void loop() {}

     

    (info from here)

     

    I was under the impression that each sketch you load to flash memory cleared the previous sketch, so I don't know if you even need to do this (unless you're just clearing it for clearing it's sake,

    although it still has the null sketch loaded . . . . )

     

    With regards the LCD, I have this one, it also uses I2C interface, there is a link on the right of the page for software. That may help.

     

    Found this too . . .

     

     

    According to what I've read, the grove item needs no pull up resistors, but there is some more info at the bottom of that page too.

     

    Of course, if the grove item hasn't got the same driver chipset as yours then I may just be talking out of my posterior (but I'm even more of a noob as my Uno is still in it's box . . . . . . . . )

     

     

    As for the rest, `i'm out until I figure stuff out myself! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • c4m4ch0
    0 c4m4ch0 over 9 years ago

    Hi,

     

    Try to install this library: LiquidCrystal_PCF8574 (Sketch/Include Library/Manage Libraries). Then you have an example (File/Examples/LiquidCrystal_PCF8574/LiquidCrystal_PCF8574_Test). If nothing appears in the LCD try to change the I2C address to 0x3f.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago

    This tutorial may be of some use

    http://tronixstuff.com/2014/09/24/tutorial-serial-pcf8574-backpacks-hd44780-compatible-lcd-modules-arduino/

     

    Data sheet on the NXP PCF8574_74A I2C I/O expander

    http://www.nxp.com/documents/data_sheet/PCF8574_PCF8574A.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nealbopper
    0 nealbopper over 9 years ago in reply to c4m4ch0

    I was all over the place today trying to figure out the x=27 code, then I found that after hours of trying to find a good sketch that would load. I used "hello world" And I got that to work. PHEW!

    Then I wanted to get the RTC date and time to show and I was running into problems there. I found a YouTube video where a guy already had the code and I copied it but it wouldn't work. DAMN! So I got creative and copied and pasted lines into the "Hello world" file and I'll be dammed. I got it to work the very first time. I was amazed! I am so green at this Arduino stuff. So now I have to add the motor controller with 2 drill motors, 4 limit switches  and a light sensor to the program and I am golden. I'm crossing my fingers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nealbopper
    0 nealbopper over 9 years ago in reply to beacon_dave

    Thanks for the response Dave. Please see the comment above. Neal