Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Radio Control Help Please (Arduino)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 419 subscribers
  • Views 1558 views
  • Users 0 members are here
Related

Radio Control Help Please (Arduino)

hank_the_electric_explorer
hank_the_electric_explorer over 9 years ago

     I am trying to upgrade a  my robot I built. I Have a IR remote control which has about a ten-twenty foot range. I am buying a new chassis and everything but I am having trouble understanding the basics of Radio control. I have googled "Arduino RC", but it is way to complicated for me. I understand the basics of Arduino coding and the bare bones of remote control but it gets a bit complicated.

 

My Questions are : Is their a easy trick I can learn with the Arduino to help get a radio controlled robot? ( Like in this tutorial with pressing a button and putting the numbers in the code)

     Is their a tutorial some where that explains a lot about Radio control that is easy and no complicated?

     (Any other suggestions for radio control)

 

 

                       

                         Any help is appreciated!

                                                                 Thanks!        

                                                                           Ben     

                              

       

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 9 years ago +1 suggested
    IR control is Radio control using the Infrared wavelengths. Adapting to other forms is easy if you understand how the IR control works. Using other wavelengths may entail different encoding methods better…
  • vandia
    vandia over 9 years ago +1 verified
    Hi Ben! First, since it's not clear from your post, I wanted to make absolutely sure you know there's a difference between radio (RF) and infrared (IR). -IR typically has wider ranger and has a much lower…
  • jw0752
    0 jw0752 over 9 years ago

    Hi Ben,

     

    Jeremy Blum has a great book called Exploring Arduino.

     

    http://www.exploringarduino.com/

     

    Chapter 11 covers using Xbee Radios to set up a wireless link. This would be just a beginning but once you have a link you can begin to program the functions of your robot. Keep us posted on your progress.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago

    IR control is Radio control using the Infrared wavelengths.

    Adapting to other forms is easy if you understand how the IR control works.

    Using other wavelengths may entail different encoding methods better suited to their frequency ranges.

     

    I cover IR radio control in one of my VY Canis Majoris posts.

    Just holler if you're interested and I'll repost it for you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hank_the_electric_explorer
    0 hank_the_electric_explorer over 9 years ago in reply to jw0752

    Thanks for pointing me in the right direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hank_the_electric_explorer
    0 hank_the_electric_explorer over 9 years ago in reply to COMPACT

    Thanks! It would help a lot if you reposted it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WarrenW
    0 WarrenW over 9 years ago

    Essentially the Radio link can easily be setup, the structure of the data can be preset to an array of data bits and these bits can be used by the receiver to turn on/off the controls. Pretty simple for on/off control.

    Now if there is a need to get a proportional system running, e.g. steering via a pot or speed control you will need to transmit a little bit more in the way of a complex signal as the analogue value of your input will need to be transferred. Again that can be handled in the structure of the data that you define and the analogue signal could then be extracted and used to drive a PWM servo system of sorts.

     

    Great to see another member exploring the Arduino platform.

    I am still getting to grips with mine.

     

    Cheers

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vandia
    0 vandia over 9 years ago

    Hi Ben!

     

    First, since it's not clear from your post, I wanted to make absolutely sure  you know there's a difference between radio (RF) and infrared (IR).
    -IR typically has wider ranger and has a much lower energy cost, but requires a line of sight from source to sensor, with something transparent as a protective shield in some cases.
    -RF can work through many materials, if you need to cover the sensor, or need to control it from different directions, where a clear path to the sensor is not practical or doable.


    Which you are using typically doesn't change your programming, other than sometimes what files must be included, because you're typically just reading a value from the digital port it's plugged into. It typically returns a number or other data to the Arduino based on the sensor being used to receive the remote. I believe there are packages for reading data from those sensors, but I always prefer to use a remote that just returns a digital number.

     

    When you use one of them, you can just use a "Case" statement, based on reading/testing what each button's value is in the serial monitor, example here if you need to know how to use the serial monitor: https://cdn-learn.adafruit.com/downloads/pdf/adafruit-arduino-lesson-5-the-serial-monitor.pdf

     

    Once you (figure out/write down) what each input from the sensor for your remote returns digitally (let's say you press "up", and it returns "3" in the monitor, you write a case statement for input 3, and do the instructions either by writing them directly under case, or calling the function/statement. A case example if you need it can be seen here: https://www.arduino.cc/en/Reference/SwitchCase

     

    Sorry if this seems a bit wordy, but I reading sensors directly when possible is usually better to customize than returning data from a package/parser, which I'm guessing is what you looked up and found to be confusing.

     

    Also, please remember to select a best answer, for whichever you believe is the best, rather than leaving the topic open.
    Good luck!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hank_the_electric_explorer
    0 hank_the_electric_explorer over 9 years ago in reply to vandia

    Thanks for clarifying this should be pretty darn easy.

     

         -Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vandia
    0 vandia over 9 years ago in reply to hank_the_electric_explorer

    It is my pleasure, Ben!


    "Mathematics is the language in which God has written the universe." ~Galileo Galilei

    I feel when we keep this in mind with electronics, it's easiest to do anything (and everything) we want to do.

    I'm having to deal with A LOT of sensors for some of my recent projects.... you can check my posts (feel free to add or follow btw!), and see I'm planning to build a mech, and have already build some other robots, for house security to email my phone if something other than my rabbits moved. :3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to vandia

    Don't confuse the poor fellow!

     

    IR is only a tiny portion of the RF spectrum (and thus has a narrower bandwidth by definition).

    It's the small area of the RF spectrum below red visible light which Herschel discovered in 1800 when doing prismatic experiments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vandia
    0 vandia over 9 years ago in reply to COMPACT

    With all due respect, going into the information you just did I feel would be more confusing and impertinent information for someone just learning....

     

    For most practical purposes, RF frequencies used refers to VHF and UHF when it comes to electronics. While you're not wrong, I felt what I told him would be most pertinent to helping him get on the right track, at least moreso than a history lesson of a broader scale.

     

    Happy Friday!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>